技术文章
即插即侧 – TEDS: 采用传感器认证插入测量
即插即用在电脑技术上已经有一段时间. 现在已经应用在专业的测量和测试领域中了. HBM 现在采用传感器电子认证技术(TEDS)来实现此项功能.TEDS(传感器电子数据表)技术可以让测量工程师在30秒内完成精确的测量任务
On-Site Loading Test of Tunnel Lining Segments in Barcelona
Read how scientists from the Technical University (UPC) carried out loading tests during the construction of the “L9” two-level subway line in Barcelona, Spain. The engineers used a very complex test procedure for analyzing the...
Displaying results 11 to 15 out of 15