测量应用报告
测量应用报告 是由独立撰稿人撰写的关于测量技术和应用的科技杂志.
RAM 成立时间是上世纪60年代.
它是由德国 Chemnitz 大学机械学院的 Dr. Martin Stockmann 博士负责编写的. 每年两期,有英文和德文版本,并通过 HBM 网站发布.
Mechanical and thermal strain
This article explains the terms "mechanical" and "thermal" stress.
Stress analysis of human teeth crowns in terms of proper occlusions
Standards of occlusion for human teeth are individually distinguishable and are determined by face shape, tooth location, the shape of the alveolar arch and the particular individual movements of the mandible during the...
Metrological analysis of stresses in a recycling machine for separating materials
Because of the constantly increasing pressure on our environment caused by solid waste and contaminants and the associated negative effect on our living conditions, the problems of technical pollution control are becoming ever...
Using HBM measurement technology in laboratory rock mechanics tests
The assessment of stability and long-term safety and integrity for the underground workings of mining and cavern construction, as well as landfill and ultimate waste disposal site construction in saltrock or travertine is based...
The suitability of turnouts with fixed switch diamonds for high running speeds – measuring subsidence and strain at Brieselang station
The design of the turnout crossings on the Hamburg – Berlin track section (single crossings with fixed switch diamonds) currently limits the running speed to 200 km/h.