HBM-Lösungen für Schiffsbau und Schifffahrt
Die Schifffahrt bildet seit Jahrtausenden die Basis für den globalen Handel. Der Ruf nach höherer Effizienz, immer stringentere Emissionsrichtlinien und neue Antriebe sorgen für neue Herausforderungen im Schiffbau weltweit.
HBM bietet Ihnen die passenden messtechnischen Lösungen, um in Entwicklung und Produktion von Schiffen, Schiffsmotoren und anderen Komponenten zukunftsfähig bleiben zu können. Zum Beispiel in folgenden Anwendungen:
Prüfen von Schiffsmotoren
Testing of ship engines
This is a standard application in engine testing, however it is often still performed by means of lever arms and force transducers – thus not meeting new requirements for measurement uncertainty budgets.
Standard HBM T10FH or T40FM torque transducers are perfect for the implementation into systems for testing of ship engines. With this well accepted technology, measurement uncertainty budgets of less than 1% for the complete test systems can be met.
See also our white paper on torque measurement of ship engines
Torque transducers from HBM for ship engine testing:
Überwachen von Gasantrieben in Systemen mit Direktantrieb
Monitoring of gas engines in direct drive propulsions
The latest international regulations, such as MARPOL annex VI, requires significant emission reductions.
An option for this is to increase the use of gas engines, instead of classic diesel engines. Gas engines burn very cleanly therefore exhaust gas cleaning is not necessary, however to do this they need to be carefully controlled by a high precision load signal.
Torque transducers directly installed on-board of ships with gas engines (or dual fuel engines), with direct drive propulsions, can automatically optimise the gas engine performance – this also guarantees the protection of the gas engine from knocking, misfiring and overload. Furthermore, this torque flange technology has been identified and is now promoted by international marine societies.
A customized version of HBM's T10FH high capacity torque transducer is now available with ATEX certification.
T10FH torque transducer with ATEX certificate for monitoring of gas engines
Überwachen von Gaskompressoren
Upgrading of high-capacity hydraulic dynamometers
High capacity dynamometers are integral part of test systems for marine engines. They are often still equipped with lever arms and force transducers; however this installation limits the measurement uncertainty.
A state of the art solution is offered by HBM: installation of a torque flange directly to the output shaft of the dynamometer is by far the more precise method of doing this.
Tests und Prüfungen von Schiffsrumpf und Schiffskörper

Ob an Bord, im Prüfstand oder am Modell: Mit HBM-Messtechnik können Sie Belastungen an Schiffsrumpf und Schiffskörper optimal testen und überwachen. Mit der kompletten Messkette aus einer Hand: Dehnungsmessstreifen, Aufnehmer, Messverstärker und professioneller Messtechnik-Software.
Lesen Sie unsere Case Study: Monitoring des Schiffsrumpf bei einem neuen Katamaran von Qinetiq
Messdatenerfassung bei Simulationen und Versuchen im Schiffsbau
Schiffe sind zum Teil gewaltigen Belastungen ausgesetzt. In speziellen Versuchseinrichtungen werden daher Experimente und Untersuchungen an Schiffsmodellen durchgeführt, um physikalische Phänomene besser verstehen zu können und die Schiffskonstruktionen zu optimieren. Leistungsstarke Messdatenerfassung ist dabei Pflicht. Führende Institute wie MARINTEK in Norwegen setzen dabei auf Messdatenerfassungssysteme von HBM:
Strukturanalyse mit hohen Kanalzahlen

Sie wollen große Konstruktionen wie z.B. Schiffe einer Strukturanalyse und Belastungstests unterziehen? Bei Messaufgaben mit hohen Kanalzahlen ist das Messdatenerfassungssystem MGCplus mit der Software catman®Enterprise erste Wahl.
Virtuelle Ermüdungstests mit nCode-Software

Die Softwarelösungen von HBM nCode helfen Ihnen dabei, die Schlüsselfaktoren zu verstehen, die die Lebensdauer und Haltbarkeit Ihrer Produkte beeinflussen. HBM nCode-Software ermöglicht Ihnen z.B.:
- Leistungsstarke Analysen schnell und effizient durchzuführen
- Ihre Analysezeiten deutlich zu senken - oft von Tagen zu Minuten
- Überdimensionierungen, überflüsige Kosten und Gewicht zu vermeiden
- Komplexe Prozesse und Analysen zu automatisieren
- Belastungsdaten einfach zu sammeln und zu verbreiten.
Verwiegen von Schiffen und weiteren Komponenten im Schiffsbau
Wenn’s auf das richtige Gewicht ankommt: Wägezellen von HBM sorgen in Waagen unterschiedlichster Art für genaue Ergebnisse. Auch als Einbaumodule erhältlich, z.B. für die Siloverwiegung.
Case Studies: Messtechnik im Einsatz im Schiffsbau
Überwachung von Unterwassersprengungen im Columbia River: : Genesis HighSpeed erfüllt höchste Sicherheitsanforderungen
Das HBM-Messdatenerfassungssystem GEN7t sorgte für eine erfolgreiche Überwachung von Unterwassersprengungen in einem ökologisch sensiblen Abschnitt des Columbia River.
Erfolgreicher Einsatz von HBM SoMat eDAQ zur Überwachung eines Schiffsrumpfs
Bei Entwicklung und Bau des neuesten Prototyps eines schnellen Landungsschiffs für das britische Militär hat QinetiQ das Messdatenerfassungssystem SoMat eDAQ von HBM als Teil des Prüf- und Auswertesystems eingesetzt.
Das schnellste Segelboot der Welt mit Messtechnik von HBM
Wenn man mit einem Boot über das Meer „fliegen“ will, bedarf es innovativer Materialien und Technologien. Der Franzose Alain Thébault setzt bei der Entwicklung seines Trimarans „Hydroptère“ auf Messtechnik von HBM, um die...
Vier mal vier - Digitale HBM-Wägezellen für Brückenwaagen
Die Westco Ltd., mit Sitz im Südwesten Englands, ist ein sehr erfolgreiches Unternehmen im Bereich des Waagenbaus. Die Qualität der von Westco angebotenen Brückenwaagen und der Wartungs- und Kalibrierdienstleistungen für Waagen...
Auf Rekordkurs...
Das schnellste Segelboot der Welt - unterwegs mit Messtechnik von HBM.