arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Kolubara Metal: Assessment of Stability

Measurement, weighing and determination of the center of gravity of mining machine superstructures using technology from HBM Test and Measurement

Kolubara Metal Vreoci in Serbia was established in 1953 as a part of Kolubara-a large industrial mining conglomerate. Kolubara Metal is a manufacturing and engineering company specializing in mining equipment, equipment maintenance, repairs, and other engineering machinery used in the mining industry. To facilitate the assembly and maintenance of mining machines, an improved method needed to be found for weighing the superstructures of mining machines. Weighing was the procedure of choice for determining the weight and location of the center of gravity on mining machine superstructures. It can be performed on different types of mining machines (bucket-wheel excavators, spreaders, mobile transfer conveyors, etc.) and can also be used on various steel structures in other industrial applications. Weighing has been carried out at Kolubara Metal since 1988. The measurement laboratory and research service was established in 2002. It was accredited in accordance with SRPS ISO/IEC 17025:2006 in 2009. Weighing of mining machines needs to be performed after a factory is built, or after major reconstruction, at periodical intervals. The overall assessment of stability of mining machines is based on weighing results (several mining machines in Serbia had previously crashed due to the center of gravity being unknown).

Weighing process

Weighing is a complex method because it involves lifting the entire superstructure (up to 50m in length and 40m in height, with a mass of 1500 t) off the ball-bearing undercarriage by means of hydraulic jacks as well as determining the individual jack loads. The method used is based on two measuring systems operating in parallel:
  • Hydraulic measurement, which measures the hydraulic oil pressure 
  • Measurement of the electrical resistance, i.e. the measured change in the resistance of a strain gauge-based force transducer
The position on the mining machine where the force transducer is installed is known as the jacking point, and it is custom designed. Mining machines usually have three or four jacking points, however, the company is able to measure six points simultaneously.

Measurement of electrical resistance

The measurement method utilizes HBM’s C6A force transducers (with capacities of 5000 KN) as well as the MGCplus data acquisition system and catman measurement software for configuring, visualizing and analyzing data.

Weight measurement & Determination of the center of gravity

The loads at the jacking points are measured online, and measured data is displayed in numerical and graphical formats. During weighing, the loads can be observed at the various points. The figure shows the moment when the superstructure is lifted off the ball-bearing undercarriage (flat line). The oscillation of the superstructure can also be observed during the measurement sequence. The center of gravity is determined using Varignon's theorem.

References & Authors

The measurement laboratory and research service has accomplished 120 weighing assignments since 2002

Authors

Branko Nikolić, MSc Mechanical Engineering
Rajko Spasojević, BSc Electrical Engineering

Related Products

No more result to load