arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Monitoring El Giraldillo in Seville

Seville Cathedral, Seville

Introduction

A monitoring system including HBK's MGCplus amplifier system was used to monitor any mechanical changes to the sculpture during restoration work.

chevron_left
chevron_right

El Giraldillo: Monitoring system

El Giraldillo is a 5 meter high bronze sculpture weighing 2000 kilos, which crowns the top of the tower of La Giralda, the Seville Cathedral. This 98 meter high tower is a former Almohaden minaret and at the time of its erection in 1184, was the highest tower in the world. As well as its decorative function, since 1568, El Giraldillo has also served as a weather vane from the highest point of the town.

Between 1999 and 2005, a monitoring system was fitted to El Giraldillo to detect any potential deterioration in the structure enabling timely restoration work to be undertaken.

The specialist construction group of the Escuela Superior de Ingenieros de Sevilla (University of Engineering) decided to use the MGCplus amplifier system to monitor any mechanical changes to the sculpture.

Working together with HBK, different sensors were installed to record the most important mechanical states connected with the mechanical behavior of the sculpture (movement, mechanical stress, bending moment, torque, acceleration). Installed above the weather vane support were three strain gage full bridges to measure bending moment and torque, accelerometers to analyze the movements of the structure and inclinometers to detect the long-term tendencies of the mast to tilt.

The wind speed, wind direction, temperature and atmospheric humidity were also measured, in order to relate the external conditions to the principal mechanical measurements. Corrosion sensors were also installed to detect possible chemical reactions at the junction points of different metals.

All measurement signals are evaluated by an MGCplus amplifier and stored on a CP42 hard disk, which can then be called up by the university via a 2.8-km WiFi link.

The basis for the success of this project is our close collaboration with our partner, HBK Ibérica, who helped enormously in setting up the sensors, cabling and measurement system.

Seville Cathedral

Technology used

Other case studies

Showing 9 of 511 items
No more result to load