Software measures multiple parameters independently of other devices
HBM’s DeviceTypeManager (DTM) for the digiCLIP amplifier provides central control for all devices in a modern production system for improved asset management.

HBM’s DeviceTypeManager (DTM) for the digiCLIP amplifier provides central control for all devices in a modern production system for improved asset management.
The software enables system operators to set up amplifiers, visualize measured values and manage device settings centrally both in the device and in the machine control system.
Integration and operation is implemented via the system control station or glob-ally via the Internet using Field Device Technology (FDT) principles, for more information visit www.fdtgroup.org/en. All aspects of modern system asset man-agement – such as system condition, machine parameters and production capacity – are available to the operator. Using these techniques the DTM is optimally matched to any device ensuring that each device is used optimally.
HBM’s digiCLIP amplifiers are used for monitoring forces and torques in produc-tion or filling processes and can be easily integrated into a production system to provide graphical displays of key information. Integration utilizes the Profibus DPV1 protocol which makes it possible to integrate any devices into a system whatever their manufacturer or fieldbus protocol.
The DTM for the digiCLIP amplifier is supplied with every module on a CD and can also be obtained free of charge from www.hbm.com/digiclip making it possible to retrofit production systems with the FDT/DTM technology.