PMX measurement system honored with MessTec & Sensor Masters Award

HBM's innovative PMX amplifier platform has been honored with second place in the Test & Measurement category at the MessTec & Sensor Masters Award 2012.

The PMX measurement system from HBM was honored at the MessTec & Sensor Masters Awards with second place in the Test & Measurement category.

The PMX measurement system from HBM was honored at the MessTec & Sensor Masters Awards with second place in the Test & Measurement category.

The new measurement system is the ideal solution for numerous metrological tasks in the production environment. True to its motto "Fit to Function," the scalable system provides the user with precisely those functionalities required for the application.

HBM's products are based on current standards such as Industrial Ethernet with real-time Ethernet protocols Ethercat and Profinet. That means PMX measurement systems are also easy to integrate into modern automation systems. The measuring amplifier processes measured signals internally in real time.

Typical applications include monitoring manufacturing processes such as fitting or pressing. The robust system is designed modularly and can be easily expanded if a plant is modified, thereby ensuring the user's investment will be secure in the future.

The honor was awarded at the MessTec & Sensor Masters event at the beginning of March in Stuttgart. The award highlights especially innovative new development products. Instead of a jury, the public decides which prizes are awarded.