Application Reports on Industrial Process Control
HBM's piezoelectric force washers enhance press-fitting of bearings, bushings and bolts
Servo-electrically driven press-fir units are increasingly used for press-fitting of bearings, bushings and bolts. Encoders and force washers are often used for recording process parameters.
Cracking connection rods - The new manufacturing process
Almost every internal combustion engine uses connecting rods to convert the linear movement of the pistons into the rotational movement of the crankshaft. If split connecting rods are used, the connection rod eye lower end must...
Monitoring small forces safely and reliably using HBM piezo force measurement technology
When testing sensitive components it is essential that small forces or torques be reliably measured. Full integrity of switches or control elements must be ensured. A typical example for an application is the final testing of...
EMG PRESSES rely on MP85A FASTpress
Ultra-modern force transducers from HBM allows French press manufacturer EMG PRESSES discovering errors that would otherwise be difficult to find.
Five test steps, one solution: FASTpress for the final inspection of highly complex steering systems
Modern steering systems in vehicles have highly complex functions – and therefore have significant influence on the driving and safety feeling.
Perfectly cut silicon wafers: digiCLIP ensures leaps in efficiency for the production of photovoltaic systems
The solar branch is booming – and therefore also the production of photovoltaic systems.
Checking rotary switches correctly: With immediate results for optimal production control
Switches and locking systems play a key role in high technology products. They are easy to operate and therefore ensure secure handling of complex products.
End-of-line testing for selector controls for automatic transmissions
DURA Automotive Systems Einbeck GmbH makes selector controls for automatic transmissions. To ensure 100 % error-free functionality and consistent high quality, a test concept was developed in cooperation with a system integrator...
“HBM Expert Discussion“: 5 questions on industrial process control
The Titgemeyer company is a leading manufacturer of vehicle components and fastening technology. Titgemeyer install their mechanical fitting technology products into automated production lines.
Switching elephants in split-second timing - HBM measurement technology for joining monitoring
HBM supplies the complete measuring system for joining monitoring in the production of switching elephants.