Technical articles

Profit from the expertise of the market leader...

Fundamental knowledge, application examples, product information – various technical articles and whitepapers from HBM on the subject of Industrial Process Control.

T40B with rotational speed measuring system and reference pulse

There are countless incremental rotational speed measurement systems available on the market. However, these systems are intended solely for measuring rotational speed. Combining rotational speed and torque measurement in a...

Spoilt for choice: piezoelectric or strain gauge based force transducers?

Two principles have become dominant in force measurement: Piezoelectric sensors and strain gauge (SG) based force transducers. When is which principle appropriate?

The key to new applications: precision

Efficient in use: S-shaped S2M force transducer. Using high-precision transducers, for example S2M from HBM, provides many benefits. Sensors offering an accuracy class of 0.02 enable force measurement chains to be designed with...

Force shunt measurement using CFW piezoelectric force washers

The measuring chain's sensitivity varies depending on the pre-stressing device's design. For example, when HBM's CPS set of pre-stressing elements is used, the CFW piezoelectric force washers' sensitivity is reduced by 7-12 %....

Measuring forces in the force shunt: Three methods used in practice

Sometimes it is of advantage to measure force in the force shunt. This article presents three methods used for measurement in the force shunt.

How does a strain gauge-based force transducer work?

The functionality, benefits and special characteristics of strain-gauge force transducers: This technical article provides the perfect introduction to the topic.

How using high-precision force transducers reduces sources of error during measurement

Using high-precision force transducers offers many benefits: Measuring chains can be designed for high overload, transducers can be flexibly used in many different measurement tasks. Moreover, sources of error during force...

FDT technology for amplifiers

In 2003, a number of prestigious companies in the automation sector established the FDT Group, in order to create a common communications and configuration interface for field devices in automation technology. We now have...

New HMI Software Solutions for Process Monitoring: A Modular System

Operability and functional control - it is just these requirements that HBM addresses with the new HMI software solutions of FASTpress Suite.

Total cost of ownership: application potentials of your test and measurement equipment

Correct, reliable measurement results are worth their money. However, when purchasing your new test and measurement equipment the mere hardware price should not be the only factor you take into account. Totally different factors...

Displaying results 1 to 10 out of 21

1

2

3

Next >