Application Reports on Weighing Technology
Load cells ensure high accuracy in latest Weigh Blending Systems
TSM Control Systems of Dundalk in Ireland is using HBM’s single point load cells to ensure high accuracy in its range of Weigh Blending Systems.
Used in Australia's largest wine-growing region: HBM's universal Z6 load cell
High humidity of the processed material and, at the same time, high temperatures: The Australian company Accuweigh relies on weighing technology from HBM for the difficult conditions of a compost plant.
Full to the brim with intelligent details: KOSME Group makes filling machines FIT®
Although it looks trivial at first, when you take a closer look at it, decanting liquids on an industrial scale is extremely complex. For example, numerous measurements and checks have to be made in fractions of a second here,...
Vage Ergebnisse – Wägezellen der Genauigkeitsklasse C6 im Test
Kunden im Einzelhandel verlassen sich auf sie und vertrauen ihnen: den Messergebnissen moderner Thekenwaagen. Kein Wunder, denn gerade die im Handel eingesetzten Waagen unterliegen der Eichpflicht und werden somit alle zwei Jahre...
Unified standards for Europe – HBM leads the way
In Europe, there are regulations and directives governing methods of measurement and test procedures for measuring instruments. MID (Measuring Instruments Directive 2004/22/EC) is a directive that assists technical harmonization...