Digital load cells for checkweighers
The digital load cells from HBM enable functionality, speed and accuracy to be optimally adapted to the requirements of checkweighers.
The load cell feeds the control electronics with a digital, scaled signal corresponding to the weight value.
The load cell electronics performs sorting tasks by means of limit values and hysteresis.
A trigger function enables an event-controlled determination of weight depending on speed, size and accuracy. In addition to their high torsional and bending stiffness, the load cells ensure good protection against mechanical loads by means of integrated overload protection in the direction of tension and compression.