Weight Indicators and Weight Controllers from HBM
HBM supplies weighing indicator for all industrial platform scales, truck or container scales. In addition, HBM offers electronic systems for process automation, e.g. for checkweigher and dosing process.
| Product | Description | ||||||
|---|---|---|---|---|---|---|---|
| AED | ![]() |
Transducer electronics for digitizing signals supplied by analog load cells
|
|||||
| DIS2116 | ![]() |
Digital weighing indicator for vehicle scales and railroad track scales
|
|||||
| DWS2103 | ![]() |
Scale display for communication with legal-for-trade load cells and electronics
|
|||||
| WE2107 | ![]() |
Mordern weighing indicator for dynamic and static applications
|
|||||
| WE2108 | ![]() |
The electronic weigher system is designed for platform scales, providing all the basic functions of a non-automatic scale or a simple counting scale.
|
|||||
| WE2110 | ![]() |
Precision digital indicator using the latest Sigma-Delta A/D converter to ensure extremely fast and accurate weight readings.
|
|||||
| WE2111 | ![]() |
Legal-for-trade weighing indicator for industrial applications - COMING SOON!
|
|||||
| RM4220 | ![]() |
Strain gage amplifier with a 4 mA to 20 mA output signal. It is easy to install, simply snapping onto standardized support rails.
|
|||||
| VKIA405 | ![]() |
Digital amplifier for connecting up to 4 strain gage load cells
|
See related articles on HBM's Weighing Electronics and Indicators
Legal-for-trade weighing systems in open automation applications
Legal-for-trade capability is mandatory in many automation environments. Which components do you need to use to guarantee that your application is legal for trade? For more information, please read our article.
Automatic weighing instruments for legal-for-trade applications: requirements and directives
Weighing technology plays an important role in many industrial applications, for example in bulk material logistics. Depending on the application, different types of automatic weighing instruments are used. What do you have to...
Preventive maintenance of weighing systems
The technological insides of scales have become increasingly complex over the past years. A consequence: When a scale fails, elimination of the problem takes longer and is likely to be more expensive. The better way: Make sure...
Protection against manipulation in weighing technology using 256-bit encryption
Protection against manipulation is among the major challenges in digital weighing technology. HBM relies on extremely secure 256-bit encryption technology. Why this is so and what are secrets behind this technology? You'll find...
Weighing and batching electronics: The Bavarian State Research Center for Agriculture (LfL) relies on HBM weighing technology
Lab-based research studies for optimizing the methane yield and managing the process control of anaerobic digestion of renewable raw materials developed an automatic filling device that continuously loads the fermenter system...
Weighing technology in process plant engineering
How to uncouple a reactor that has to be chilled or heated in the course of a process? What should the approach be if the mixer has to be fitted with a stirrer? How to design the platform if the mixer has to be supported on...