- HBM Measurement Engineering
- Calibration Service
- Service applications
- Support
- Repairs
- Parts logistics and leased equipment
- Seminars and training sessions
- Service contracts
Calibration Laboratory at HBM: Germany's first accredited DKD calibration lab
Welcome to the HBM calibration laboratory - one of the best known and most capable calibration labs of its type worldwide!
In 1977, the first accredited German Calibration Service (DKD) Calibration Laboratory was based at HBM. Since then, it has become one of the best known and most capable calibration labs of its type. Accreditation to DIN EN ISO/IEC 17025 covers the measured quantities: force calibration, pressure calibration, torque calibration and voltage ratio mV/V calibration.
HBM Calibration Laboratory - accredited by DKD
The German Calibration Service (DKD) is an association of calibration laboratories which are obliged to regularly demonstrate their competence and quality of service to the accreditation authorities in order to maintain their accreditation status.
Accreditation of our calibration laboratory is your guarantee that calibration is performed in accordance with mandatory standards and guidelines. A calibration certificate is certified proof of traceability.
Working Standard Calibration
Working standard calibration means it is the responsibility of the calibration laboratory to carry out the testing. The traceability must be explicitly documented. At HBM this is done by reference to DIN EN ISO 10012. Under certain conditions, working standard calibration is possible on site.
Traceability to ISO9000
Every company wishing to attain ISO9000 certification or already possessing it has to prove traceability to National Standards. This is intended to ensure "proper" measurement.
Traceability is proven when an item of test equipment or a measuring device has been calibrated with a reference, the calibration of which in turn can be traced back, in an unbroken chain, to the National Standard.