Calibration Facts
Calibration is...
…determining and documenting the deviation of a measuring instrument display from the correct value of the measured quantity.
Calibration is not just a binding specification in a standard, such as ISO 9001, it also helps to obtain measured values than are demonstrably reliable.
With calibration, these are continuously traced back to the national standard (traceability) and internationally comparable and globally recognized measured values are obtained.