© rc10de / photocase.com

Industrial Amplifiers - Software and Firmware Downloads

Please enter your email address.

If you already have an account with HBM.com, log in here using your email address to get unlimited access to HBM's complete technical documentation.

PMX

Description Version Build Size Date
HBM common API
The HBM common API enables users to develop their own PC software application using Microsoft Visual Studio, to integrate HBM DAQ systems QuantumX, SomatXR, PMX and MGCplus.
The download includes the API as well as documentation and examples.
2.0R2   9 MByte 06/2015
HBM LabVIEW Driver
The driver allows to integrate QuantumX, SomatXR, PMX and MGCplus in LabVIEW.
Please see the Release Notes for futher details and requirements.
2.0.2   8 MByte 07/2015
PMX 3D-modell
This project is a 3D-modell as STEP-files for CAE
 
    4 MByte 12/2012
PMX CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
2.00   27 MByte 12/2013
PMX Codesys Examples
This is a collection of Codesys software achives for typical requirements around PMX. They show a step-by-step solution up to the running project in Codesys and PMX. Available languages: german, english.
  • PMX Web-visualisation
  • PMX in CAN-Master and -Slave mode
  • PMX with CAN-modules for temperature and climate measurements
  • PMX with Client-Server communication via TCP/IP
  • PMX with integrated data-storage on internal memory or USB-stick
Legal notice: The examples given are intended to illustrate the solution and integration into PMX. The examples do not imply any warranty or guarantee.
 
1.0   69 MByte 02/2015
PMX CodesysV3
Archive including all current files for CodeysV3.5SP3 software installation and PMX-Package. Included are also PMX Codesys examples for an easy Startproject, Codesys-WebVisualisation, PMX-CAN-interface support for CAN-devices(e.g.SomatCR) and CAN-Master-Slave communication. The examples do not imply any warranty or guarantee.
1.02   439 MByte 01/2014
PMX EDS files (Ethernet/IP)
PMX device description file for Ethernet/IP.
 
0.24   0.1 MByte 02/2015
PMX Example EtherCat Project
This example considers a simple test assembly including a Beckhoff PLC CX1020 and a PMX. In this example, consistent (coherent) data are written and read via the EtherCat and shown is a visualization panel. Legal notice: The example given is intended to illustrate the integration of PMX into Beckhoff TwinCat software via EtherCat. This example does not imply any warranty or guarantee.
 
    1 MByte 04/2014
PMX Example Ethernet/IP Project
This example considers a simple test assembly including a AlanBradley PLC Compact Logix L24ER and a PMX. In this example, consistent (coherent) data are written and read via the Ethernet/IP. Legal notice: The example given is intended to illustrate the integration of PMX into AlanBradley's software RSLogix 5000 via Ethernet/IP. This example does not imply any warranty or guarantee.
 
    2 MByte 04/2014
PMX Example LabView 2011
This example uses the internal PMX command-set and illustrates how to connect, read, write, measure with PMX.
Requirements: LabView 2011
It has a linewriter included and can sent/receive single commands to/from PMX.
All commands are described in the PMX manual.
This example does not imply any warranty or guarantee.
LabVIEW is a registered trademark of National Instruments Corporation.
1.1   1 MByte 02/2015
PMX Example LabView 2012
This example uses the internal PMX command-set and illustrates how to connect, read, write, measure with PMX.
Requirements: LabView 2012
It has a linewriter included and can sent/receive single commands to/from PMX.
All commands are described in the PMX manual.
This example does not imply any warranty or guarantee.
LabVIEW is a registered trademark of National Instruments Corporation.
1.1   1 MByte 02/2015
PMX Example Profinet Project
This example considers a simple test assembly including a Siemens CPU315-2 PN DP and a PMX. In this example, consistent (coherent) data are written and read via the Profinet. Legal notice: The example given is intended to illustrate the integration of PMX into Siemens' Step7 software via Profinet. This example does not imply any warranty or guarantee.
 
    2 MByte 04/2014
PMX Firmware and WebServer
Archive including all current files for firmware and PMX WebServer. To update firmware and WebServer the existing WebServer in the PMX can be used (no additional software or hardware needed).
2.02   33 MByte 05/2015
PMX GSDML files (ProfiNet)
PMX device description files for ProfiNet RT and IRT.
 
2.3   0.1 MByte 02/2015
PMX TechNotes

This is a collection of technical application reports for typical requirements around PMX.
They show a step-by-step solution up to the running project in PMX.
Available languages: german, English and French.

  • PMX with Codesys and Codesys WebVisualisation
  • PMX as CANmaster and CANslave (read/write CAN messages)
  • PMX with IEPE-sensors, T40 torque-sensors, Piezoelectrical-sensors
  • Read sensor signals via CAN, e.g. torque/speed (T12), temperature, climate
  • PMX with calculated channels:
    • Event-counter, X-borders, tolerance-band, tolerance-windows, result-force
    • Mechanical work, stress-analysis
    • Combined Triggeroutput
    • 6x6 Matrix-compensation (noise reduction for Multi-Component sensors)
    • PID-regulator, PT100-measurement
  • PMX integration in a PC-network (Windows or Linux)
    • Using the PMX dotNET-API
    • Using the PMX command-set under LabView
    • Using PMX together with catman for DAQ
  • PMX integration in an automation-network
    • EtherCat and TwinCAT(Beckhoff)
    • ProfiNet (Isonchronus-Real-Time (IRT) and Simatic-manager (TIA-portal, Siemens)
    • Ethernet/IP and RSLogix (Rockwell Automation)
  • PMX NTP-synchronisation with QuantumX
  • PMX with internal Dats-Storage or on USB-Stick

Legal notice: The examples given are intended to illustrate the solution and integration into PMX.
The examples do not imply any warranty or guarantee.


 
1.2   62 MByte 04/2015
PMX XML files (EtherCat)
PMX device description file for EtherCat.
 
1.3   0.1 MByte 02/2015

PME Series (including MP85A)

Description Version Build Size Date
MP85A CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   19 MByte 08/2011
PME CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
    30 MByte 08/2011
PME EDS files
EDS files for PME (MP01, MP30, MP55, MP60, MP85).
 
1.01   0.03 MByte 11/2011
PME FASTpressSuite CD

PME assistant, firmware loader and USB driver (for Windows XP, Windows Vista and Windows 7/8) for comfortable setup and visualisation. For smooth operation of modules with CAN interfaces, use the PEAK USB-to-CAN dongle. All required drivers are included and will be installed during startup.

This download includes:

  • PME-Assistant (V3.4.206)
  • PME-Firmware Loader (V1.1.7)
  • IPM data conversion (V1.1)

... and the demo versions of:

  • EASYteach (V1.0.5.10)
  • MP85A-Toolkit (V1.0.5.12)
  • EASYmonitor CE (V1.1.1.1)
  • INDUSTRYmonitor (V1.2.1.10)

You can start those demo versions up to 25 times for free. To buy the full licence please visit the HBM shop or ask your local HBM representative.


1.50   163 MByte 07/2015
PME Firmware for hardware version 1.xx
For PME hardware version 1.xx (MP01-MP70) and all MP85/DP! For newer devices, please use the PME firmware for hardware version 2.xx on this page. Archive including all current firmware files for modules of the PME series. The appropriate firmware loader is part of the PME assistant. The zip file has to be extracted into the PME assistant directory. It includes following firmware versions:
  • MP01 Version 1.12
  • MP30 Version 1.04
  • MP30DP Version 1.04
  • MP55 Version 1.42
  • MP55DP Version 1.42
  • MP55DPS6 Version 1.42
  • MP60 Version 1.18
  • MP60DP Version 1.18
  • MP70DP Version 1.05
  • MP70DPS7 Version 1.05
  • MP70S7 Version 1.05
  • MP85 Version 1.10
  • MP85DP Version 1.10

 
HW1   1 MByte 05/2007
PME Firmware for hardware version 2.xx
For PME hardware version 2.xx (MP01-MP70) and all MP85A/ADP! For older devices, please use the PME firmware for hardware version 1.xx on this page. Archive including all current firmware files for modules of the PME series. The appropriate firmware loader is part of the PME assistant. The zip file has to be extracted into the PME assistant directory. It includes following firmware versions:
  • MP01 Version 2.00
  • MP30 Version 2.02
  • MP30DP Version 2.02
  • MP55 Version 2.06
  • MP55DP Version 2.06
  • MP55DPS6 Version 2.02
  • MP60 Version 2.00
  • MP60DP Version 2.00
  • MP70DP Version 2.00
  • MP70DPS7 Version 2.00
  • MP70S7 Version 2.00
  • MP85A Version 2.36
  • MP85ADP Version 2.36
  • MP85A-S Version 2.36
  • MP85ADP-S Version 2.36


HW2   2 MByte 07/2013
PME MP85ADP(-S) Example Project
Program example to the communication of the HBM process-controller MP85 with a Siemens Siemens CPU317-2 DP:
The example of the communication with the MP85A about Ethernet please unzip recursive in the ZIP archive (relatively stored paths). The program sends and receives data by means of the functions AG_send and AG_Recv (FC5 and FC6). It are sent 10 bytes to the SPS and 14 bytes should be received again. In this project the Siemens CPU317-2 DP has the IP address 172.21.64.250. The IP address of the MP85 is 172.21.64.253 (port 4020). A description with program-code and comments is shown in the documents „OP1_MP85A_Eth-Com-CPU317-2 DP.pdf “
Legal notice: The example given is intended to illustrate the integration of the MP85ADP(-S) into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.
 
    2 MByte 07/2015
PME MP85ADP(-S) Example Project
Example-Sequence to read and write consitent data as well an example to read and write the workpiece-id via Profibus-DPV1 with Siematic Step7:
This basic example shows the transmission of measuring-value and Control-word (Float data format) from the MP85ADP(-S) via Provibus-DP interface to a master (e.g. Siemens PLC). Programming is done in Step7 Siemens software using the function blocks for reading (SFC14) and writing (SFC15) MP85ADP data. Further more the example contains reading and writing the workpiece-id via the Profibus DPV1-function using the function-blocks for reading (SFB52) und writing (SFB53) to MP85ADP(-S). A description with program-code and comments is shown in the documents „OB1_DPV1_Werkstueck_de.pdf“ and „OB1_DPV1_Werkstueck_en.pdf“.
Legal notice: The example given is intended to illustrate the integration of the MP85ADP(-S) into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.
 
    6 MByte 07/2010
PME Profibus DP
PROFIBUS DP master file for PME: (MP30DP, MP55DP, MP60DP, MP70DP, MP70DPS7,MP85MP). German version: GSD file, English version: GSE file.
 
1.20   0.03 MByte 07/2013
Sequence for reading the curve memory via ProfibusDPV1 using Simatic Step7
The basic sequence of transmission of measured value (Float data format) from the MP85ADP curve memory via the Profibus-DP interface to a master (e.g. Siemens PLC) is shown in this file.
 
    1 MByte 07/2015

DT85

Description Version Build Size Date
DT85 Firmware
Archive including current firmware file and instruction for DT85. Update on DT85 is necessary when using MP85(A)(DP) with firmware 2.16 or higher.
2.15   1 MByte 03/2012
DT85 Update
Firmware update for Windows 95/98, ME, NT, 2000 and XP. Unzip the downloaded ZIP-file and read the information in the pdf file.
 
II   4 MByte 06/2007

digiCLIP

Description Version Build Size Date
digiCLIP Assistant
digiCLIP Assistant, Firmware Loader and USB Driver (for Windows XP, Windows Vista and Windows 7/8) for easy setup of digiCLIP modules and for visualization. For smooth operation of modules with CAN and DeviceNet interfaces, use the PEAK USB-to-CAN dongle. For Profibus operation Hilscher and Siemens CP5511/12 and CP5711 is supported - to handle digiCLIP firmware-updates via CP5711 digiCLIP-modules have to be equipped with a adapted bootloader which is implemented starting with following serial-numbers: (DF30DP: 816711801 / DF31DP: 817427801). All required drivers are included and will be installed during startup.
2.6.2   39 MByte 05/2015
digiCLIP CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   42 MByte 08/2011
digiCLIP DTM setup for DF30DP and DF31DP
Contains the installation of the DeviceDTM in German and English for Windows 2000/XP/Vista/Windows7/Windows8 operating systems.

Prerequisite for using digiCLIP DTM setup is the installation of a frame application (e.g. FDT container, PACTware) - not included in this download.
1.2.0.166   13 MByte 12/2010
digiCLIP EDS files (CAN) for DF30CAN and DF31CAN
EDS files for digiCLIP DF30CAN and DF31CAN.
 
1.36 / 1.20   0.01 MByte 06/2014
digiCLIP EDS files (DeviceNet) for DF30DN and DF31DN
EDS files for digiCLIP DF30DN and DF31DN.
 
1.12   0.02 MByte 05/2015
digiCLIP Example DeviceNet Project (Omron PLC)
The CX-Integrator example program shows the basic test setup of a digiCLIP DF31DN connected to an Omron Sysmac CJ1M SPS with a CS1/CJ1 DRM21 fieldbus controller. In this example, consistent (coherent) data is read and written over the DeviceNet. The DF30DN operating manual provides all possible commands and values. This example does not imply any warranty or guarantee.
 
    1 MByte 07/2015
digiCLIP Example on a CANOpen application
This applicatin is to describe an example of a small-scale digiCLIP amplifier application in a CAN network using a CANopen based PLC. In this application, load cells implemented as strain gage full bridges are used for determining the filling level in a tank and taring it to 0 ... 100% using a PLC connected to the digiCLIP. This example does not imply any warranty or guarantee.
 
    1 MByte 07/2015
digiCLIP Example Profibus Project
This example considers a simple test assembly including a Siemens CPU313-2DP and a DF30DP/DF31DP (digiclip). In this example, consistent (coherent) data are written and read via the Profibus with SFC14 and SFC15. As an additonal programming the parametercontainer is programmed to configure the DF30DP in the cyclic data exchange. To read configurations with DPV1 the Siemens function block SFB52 (PNO AK1131)is programmed, too. All commands and values for the configuration are shown in the official manual. Legal notice: The example given is intended to illustrate the integration of the DF30DP into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.
 
    6 MByte 07/2015
digiCLIP Firmware for DF30 and DF31

Archive including all current firmware files for modules of the digiCLIP series. The appropriate firmware loader is part of the digiCLIP assistant. The zip file has to be extracted into the digiCLIP assistant download directory.

DF30CAN version 1.44
DF31CAN version 1.28

DF30DP version 1.42
DF31DP version 1.28

DF30DN version 1.12
DF31DN version 1.12


    1 MByte 05/2015
GSD/GSE files for digiCLIP DF30 and DF31
GSE/GSD files for digiCLIP DF30DP and DF31DP.
 
1.34   0.003 MByte 12/2012

Clip

Description Version Build Size Date
Clip CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   17 MByte 03/2012

MGA II

Description Version Build Size Date
MGA II CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   19 MByte 03/2012

PACEline CMD

Description Version Build Size Date
CMD Assistant
CMD Assistant for Windows 2000, XP, Vista, Windows 7 and Windows 8. Allows the easy setup of CMD modules, visualization and process-data storage. All required drivers are included and will be installed during startup. Starting with assistant-version 1.2.4.0 only CMD with firmware 3.0 and higer can be used. Devices with firmware 2.9 and lower are shown in the device-scan but marked red with a note for firmware-update. Please do also a firmware-update for those devices, for features see release-notes.
1.2.6.0   79 MByte 11/2011
CMD CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   18 MByte 10/2011
CMD Firmware
Archive including all current firmware for all modules of the CMD series (CMD600 and CMD2000).
Please use "CMD Firmware Updater for Version 3.62 and higher" on this page.
3.69   0.2 MByte 05/2015
CMD Firmware Updater for Version 3.62 and higher
Copy all files in one folder and start the file CMD600_Updater.exe
 
1.00   0.4 MByte 07/2014
CMD Firmware Updater for Versions up to 3.51
Start the Setup-file and follow the instructions.
1.00   2 MByte 12/2013
CMD LabView driver and example project

To simplify the use of CMD meauring amplifier a complete support for communication in form of a Labview driver is available, respectively Labview programs/subroutines called virtual instruments (VIs).
The purpose of this document is to explain in detail all aspects of the Labview CMD driver:

  • Driver structure
  • VI blocks
  • Application example – getting started

The CMD driver is completely written in Labview Professional Development System. In order to use the drivers the user will need Labview version 9.0.1 or later.
This example does not imply any warranty or guarantee.


 
    3 MByte 07/2015
CMD Siemens Step7 example project
This Siemens Step7 example describes a project to connect the type CMD measuring amplifier from HBM GmbH to a Siemens S7-315-2 PN/DP CPU via UDP and store the measured values transmitted via UDP in a data module. The measured values are to be read and processed with up to 1000 Hz via UDP. HBM does not guarantee the completeness and correctness of this example.
 
    3 MByte 08/2011

MVD and MVD SCOUT55

Description Version Build Size Date
MVD CAE data for Eplan Electric P8
This project is a macro-project and contains CAE data for Eplan Electric P8.
 
1.00   19 MByte 03/2012
MVD Scout Assistant
System-CD for MVD and MVD SCOUT55 modules.
 
2.2   40 MByte 09/2008

TEDSdongle

Description Version Build Size Date
IEEE Code for TEDS
Conversion template containing the IEEE codes for TEDS of all HBM transducers.
 
    0.002 MByte 12/2013
TEDSdongle Setup
TEDSdongle Setup
 
3.4.0.6   33 MByte 01/2013

Related Pages

TechNote

Important update information for users of T12, PME and digiCLIP software

Read the TechNote about HBM software on multicore PCs with PEAK-CAN-USB dongle and CAN-driver