Force strain and pressure transducers based on foil type strain gauges as well as the piezoelectric principle for the use in industrial applications
Sensorics in industrial processes more and more require both fast date processing and at the same time very accurate measurement. This is because manufacturers expect consistently reliable quality control in their production. HBM force, strain and pressure transducers measure static and dynamic loads, according to the need of the specific measuring task, using latest technology.