Notas de aplicación sobre medición de par
HBM es el referente mundial en tecnología de medición de par. Los transductores de par de HBM garantizan resultados fiables en bancos de pruebas, operaciones de calibración y control de la producción. Por ejemplo, en las industrias del automóvil y construcción naval, en el sector de generación de energía (para medir el par de los generadores) y en otros muchos campos de aplicación.
Consulte las últimas notas de aplicación sobre tecnología de medición de par de HBM:
Accurate measurement data for Sisu Axles’ product development with HBM T40 torque transducers
For developing more durable and more capable axles, Finnish manufacturer Sisu Axles equipped its new test stand with torque transducers from HBM.
HBM on the test bench: Allison Transmission puts HBM to the test
Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...
Better driving thanks to PME
For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...
Optimización del algoritmo de control de INVT con el transductor de par T10F
La empresa china INVT utiliza el transductor de par T10F y los amplificadores MP60 de HBM para medir el par y la velocidad de un motor eléctrico controlado por un variador de frecuencia (VF), con el fin de optimizar su...
Efficient vehicle drives with measurement technology in the original component
Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...
Long service life and short standstill times with HBM measurement technology
HBM supports highly promising growth markets such as wind energy with state-of-the-art measurement technology. Complete solutions are required to increase the efficiency of wind power plants with HBM measurement technology from...
On test: Generators for wind turbines from The Switch
More precise measurement results with a torque flange from HBM
T40 torque transducer in APL test bench
The independent test bench service provider APL has over 70 state-of-the-art motor and component test benches, and relies on HBM measurement technology.
HBM measurement technology on the test stand: Dynamic torque measurement in water turbines
How can torque be measured more reliably and efficiently? A well-known manufacturer of test stands for water turbines trusts in a new concept: Instead of using a force transducer to measure torque indirectly through the restoring...
Siemens: Dynamic truck rear axle transmission test rig for SCANIA
As an automotive industry partner, Siemens A&D, in its vehicle test and inspection systems division provides innovative solutions for testing vehicles and vehicle components throughout the world. By using the latest HBM torque...
Displaying results 1 to 10 out of 15