Notas de aplicación en tecnologia de pesaje
An idea for tomorrow's traffic: who overloads pays more
The idea of tolls differentiated by the road damage caused is currently tested using a prototype in Romania. On board: HBM measurement technology.
Weighing a giant tortoise using load cells from HBM
Why do the shells of giant turtoises have such widely-varying shapes on different Galapagos islands? A research project in the Netherlands should answer this question by using HBM measurement technology.
Optimum use of resources in MDF production systems
The production systems for wood-based material panels of the Eppinger Dieffenbacher Group are in worldwide demand. The group has decided to use HBM’s digiCLIP digital industrial measuring amplifier and load cells in the fiber...
Teltek dynamic scales for the right quantity of fish in the pack
Teltek has just supplied a new in-house scale to a fish factory belonging to frozen food manufacturer Espersen in Lithuania. It will be an important part of the production line, ensuring that every pack of frozen fish contains...
Measuring Mudslides: Tracking Extreme Forces
Tons of debris, rush precipitously down mountainsides into valleys during mudslides. To better understand the forces at work, the Research Organization WSL is using a special scale with measurement technology from HBM.
Las células de carga de alta precisión garantizan el control de calidad en numerosas plantas cementeras chinas
XCMG, la constructora más importante de China, ha emprendido un programa de desarrollo destinado a optimizar el control de calidad en sus plantas cementeras mediante la instalación de distintas células de carga de HBM.
Gemstones make LEDs glow
LEDs, photovoltaic cells, jewelry – artificial gemstones such as sapphire crystal are used in the production and development of these products. The crystals are grown in special furnaces. Chinese manufacturers use HBM load cells...
Bühler nombra a HBM “proveedor preferente” a HBM por su calidad y puntualidad
El lema de Bühler es “Innovaciones para un mundo mejor”. Esta compañía suministra equipos, sistemas y servicios para el procesamiento de alimentos básicos en más de 140 países. Del mismo modo que sus clientes le exigen la más...
Idento Operations uses HBM load cells for intelligent feed systems
Idento from the Netherlands makes special measuring units for weighing feed quantities for pigs and cattle. Idento uses hermetically-sealed load cells from HBM for its measuring units, and they have turned out to be able to...
Dosificación óptima en todo momento: módulos de instalación RTN en un nuevo silo de conglomerante de CEMEX Austria
CEMEX Austria utiliza la tecnología de pesaje de HBM en su nuevo silo de conglomerante, para garantizar una mezcla y dosificación óptimas del mortero autonivelante de anhidrita.
¿Quiere ver su aplicación en esta sección?
¡Comparta con nosotros su nota de aplicación de productos HBM!