Case studies on agriculture
Idento Operations uses HBM load cells for intelligent feed systems
Idento from the Netherlands makes special measuring units for weighing feed quantities for pigs and cattle. Idento uses hermetically-sealed load cells from HBM for its measuring units, and they have turned out to be able to...
La célula de carga universal Z6 de HBM aplicada en la comarca vitivinícola más grande de Australia
Los altos índices de humedad del producto procesado junto con las altas temperaturas son las difíciles condiciones básicas de una instalación de compostaje en las que la empresa australina Accuweigh emplea la tecnología de pesaje...
Weighing and batching electronics: The Bavarian State Research Center for Agriculture (LfL) relies on HBM weighing technology
Lab-based research studies for optimizing the methane yield and managing the process control of anaerobic digestion of renewable raw materials developed an automatic filling device that continuously loads the fermenter system...
Too much fertilizer? A globally unique test bench for investigation and analysis
Cemagref, the French Institute for Agricultural and Environmental Engineering Research is a specialist in spreading fertilizer at one of its nine sites in Montoldre. The equipment to chart the spread of the fertilizer as it is...
Separating wheat from the chaff - quality control using HBM weighing technology
Cereal and grains are grown worldwide, traded on commodities markets and transported in complex logistics chains to the manufacturing sector. Apart from the quantity, it is primarily the quality of the raw material that decides...
Want to see your application here?
Share a case study of your HBM product with us!