Notas de aplicación
Bucher Leichtbau uses HBM test and measurement technology to test airworthiness of galleys
Bucher Leichtbau AG, Switzerland, is a leading manufacturer of galleys and cabinets installed in passenger aircraft and therefore places its trust in stringent testing of its modules to ensure their airworthiness. In the test...
Advanced lightning warning system protects spacecraft launches at Kennedy Space Center
Using HBM transient recorders and digitizers, HBM has designed a lightning monitoring system for Kennedy Space Center in Florida. The system enhances the safety of operations such as the launching of rockets by ensuring that the...
Static component testing of a drive module with MGCplus
The BEPICOLOMBO mission: The European Space Agency (ESA) and the Japanese Space Agency ISAS/JAXA want to explore Mercury – with a drive module and two separate space probes that will orbit around the planet.
HBM makes fuselage assembly safer for modern commercial aircraft
The construction of modern commercial aircraft today increasingly involves the use of innovative composite materials such as GRP or GLARE (glass-fiber reinforced aluminum). The handling of these materials during assembly sets new...
Latest Lynx lands safely following development tests
AgustaWestland has conducted a series of tests on the undercarriage of the future Lynx naval helicopter using HBM’s data acquisition equipment to ensure superior operational landing performance.
Displaying results 1 to 5 out of 15
Aplicaciones típicas
- Pruebas de fatiga estáticas y dinámicas (construcción completa)
- Ensayo de función y carga de los componentes
- Monitorización y valoración del control de fatiga de materiales
- Análisis de carga estática, fatiga o resistencia de endurecimiento
- Pruebas de choque con tren de aterrizaje
- Pruebas térmicas y de medio ambiente
- Pruebas de túnel de viento y aerodinámicas