Notas de aplicación
Next generation aircraft: Composite structures research with optical strain gauges
The Japan Aerospace Exploration Agency (JAXA) has relied on HBM’s data acquisition technology to investigate the structural health of recently developed aircraft made with composite materials.
A "lifestyle" airplane for take-off and landing on the ground, on water and snow
Making flying a pleasure again: This is the aim of the new, ultra-modern AKOYA light airplane. On-board safety and comfort is ensured through the use of strain gauges from HBM and the ultra-rugged SoMat eDAQlite data acquisition...
Apertura segura de un paracaídas: galgas extensométricas de HBM a bordo de un cohete experimental
Todos los años, un equipo de la asociación aeronáutica "CLES-FACIL" desarrolla un cohete experimental para estudiar cuestiones científicas de primera magnitud. "CLES-FACIL" ha utilizado las galgas extensométricas de HBM en un...
El régimen de pruebas estructurales integradas de BAE Systems favorece las prestaciones del F-35
Las pruebas estructurales integradas y el proceso de eliminación de riesgos del FTI de BAE Systems contribuyen a las prestaciones del nuevo F-35 Joint Strike Fighter.
Bucher Leichtbau emplea tecnología de pruebas y medición de HBM para comprobar si sus galeras son aptas para la navegación aérea
La empresa suiza Bucher Leichtbau AG es un fabricante líder de galeras y compartimentos para aviones de pasajeros. Lógicamente, somete sus módulos a las pruebas más exigentes para garantizar que sean idóneos para la navegación...
Advanced lightning warning system protects spacecraft launches at Kennedy Space Center
Using HBM transient recorders and digitizers, HBM has designed a lightning monitoring system for Kennedy Space Center in Florida. The system enhances the safety of operations such as the launching of rockets by ensuring that the...
Static component testing of a drive module with MGCplus
The BEPICOLOMBO mission: The European Space Agency (ESA) and the Japanese Space Agency ISAS/JAXA want to explore Mercury – with a drive module and two separate space probes that will orbit around the planet.
HBM makes fuselage assembly safer for modern commercial aircraft
The construction of modern commercial aircraft today increasingly involves the use of innovative composite materials such as GRP or GLARE (glass-fiber reinforced aluminum). The handling of these materials during assembly sets new...
Latest Lynx lands safely following development tests
AgustaWestland has conducted a series of tests on the undercarriage of the future Lynx naval helicopter using HBM’s data acquisition equipment to ensure superior operational landing performance.
Ballistics & Missile Testing: Making Sure it is Recorded the First Time
With once in a lifetime tests, you want to make certain that you capture the event. Genesis HighSpeed by HBM has the tools and experience to do just that. For over 35 years, Genesis HighSpeed has been a market leader in high...
Displaying results 1 to 10 out of 19
Aplicaciones típicas
- Pruebas de fatiga estáticas y dinámicas (construcción completa)
- Ensayo de función y carga de los componentes
- Monitorización y valoración del control de fatiga de materiales
- Análisis de carga estática, fatiga o resistencia de endurecimiento
- Pruebas de choque con tren de aterrizaje
- Pruebas térmicas y de medio ambiente
- Pruebas de túnel de viento y aerodinámicas