Notas de aplicación

Serving a greener automotive industry

The demands on energy efficiency and the CO2 balance of motors are constantly increasing. A manufacturer of water, oil and vacuum pumps for thermal engines therefore decided to use a complete solution from HBM.

Testing of electric and hybrid cars: HBM, a key partner for the French company, GreenMot

Tests on electric motors present a new challenge when it comes to measurement. French testing company GreenMot has opted for HBM's innovative eDrive testing solution.

HBM on the test bench: Allison Transmission puts HBM to the test

Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...

Better driving thanks to PME

For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...

Reducing the cycle time with FASTpress when assembling cylinder heads

In combustion engines, valve seats and valve guides are subjected to special loadings. There are thermal loads as well as mechanical loads, produced by the ignition pressure or by the valve disk coming down hard when closing....

Volvo Construction Equipment (CE): mejora del consumo de combustible de cargadoras mediante pruebas exigentes y el sistema de adquisición de datos SoMat eDAQ

Volvo Construction Equipment (CE) emplea el sistema de ensayo SoMat eDAQ de HBM para probar sus prototipos de cargadoras en condiciones extremas.

La movilidad eléctrica en el carril rápido: mejoras de eficiencia para la conducción del futuro

Durante mucho tiempo, los vehículos eléctricos solo han tenido un desarrollo marginal. Sin embargo, el progresivo agotamiento de los recursos petroleros, la consiguiente subida del precio de los combustibles y la mayor conciencia...

Tiempos de reacción en condiciones de tráfico: un innovador método de análisis utiliza tecnología HBM

En medio del tráfico, reaccionar suele ser cuestión de milésimas de segundo. ¿Cómo reaccionamos al volante ante una situación de peligro? Con ayuda de la tecnología de medición de HBM, el ingeniero suizo Mauro Balestra ha...

Efficient vehicle drives with measurement technology in the original component

Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...

Aluminum alloy wheels - tested with QuantumX MX410 data acquisition modules

Shorter development times - this is the aim of all technology companies worldwide. BORBET, the world's leading manufacturer of aluminum wheels shows how it is done: Using a smart system of efficient tests. Always on board: HBM...

Displaying results 1 to 10 out of 36

1

2

3

4

Siguiente >