Structural health monitoring with HBM

Civil Engineering Testing with HBM: Viable measurement results for you

For the planning and design of buildings, evaluation of damage or implementation of fatigue tests: viable measurement results count in structural health monitoring.

Products and services around structural health monitoring

Can a bridge still be permanently used? Can a building be restored? Will a structure hold firm even if certain parts are removed or altered? Is a specific construction material suitable for the requirements? Can earthquake tests be simulated?

These and many other questions arise within the field of structural health monitoring. The answers are provided by the measurement products and services from HBM: with strain gages, transducers, amplifiers and measurement technology software from one source—for your demanding measurement technology tasks in structural health monitoring. Our products are enhanced by a professional service portfolio covering installation, commissioning and maintenance for your measurement technology on site.

Do you have any questions on structural health monitoring with HBM? Let us help you. Contact HBM

Regardless of whether you need to measure pressure, force, displacement, temperature, oscillations, acceleration and numerous other measured quantities in structural health monitoring: HBM transducers and amplifiers offer you results that you can trust.

HBM measurement technology for structural health monitoring provides viable measurement results—be it for planning, deformation measurement, movement monitoring and long-term monitoring of structures such as:

  • Buildings
  • Bridges
  • Dams
  • Tunnels
  • Roads

Application reports on structural health monitoring with HBM:

Static and dynamic load tests completed in record time: SHP opts for QuantumX from HBM for bridge monitoring

Only five days were allowed for static and dynamic load tests on a new bridge across the Nitra river to be conducted by the Czech company SHP. One of the secrets behind the success: utilization of HBM's QuantumX data acquisition...

Dosificación óptima en todo momento: módulos de instalación RTN en un nuevo silo de conglomerante de CEMEX Austria

CEMEX Austria utiliza la tecnología de pesaje de HBM en su nuevo silo de conglomerante, para garantizar una mezcla y dosificación óptimas del mortero autonivelante de anhidrita.

Un proyecto de voladura subacuática cumple los más estrictos requisitos de seguridad gracias a los equipos Genesis de HBM

Dos contratistas estadounidenses recurrieron a los equipos de adquisición de datos de alta velocidad Genesis de HBM para monitorizar la voladura subacuática de un tramo de alto valor ecológico del río Columbia, cerca de St....

Control de carga en el estadio Olympiahalle de Múnich

Hoy en día los conciertos, sobre todo los de música pop, son cada vez más desmesurados. En consecuencia, el equipo de luces y sonido que utilizan los artistas es grande y pesado. Sin embargo, los techos y pórticos de iluminación...

Keeping an eye on the effects of heavy goods traffic: Long-term monitoring on a motorway bridge

Increasing heavy goods traffic is a constant endurance test for the approximately 38,000 bridges on the German motorways and main roads. In order to investigate these effects, the Federal Highway Research Institute (BASt)...

Load testing on the Ponte della Costituzione in Venice

The Ponte della Costituzione is designed by the Spanish architect Santiago Calatrava and became the fourth bridge over the Grand Canal in Venice when it was inaugurated in September 2008. HBM Italy worked with Verona-based Veneta...

Tunnel monitoring with QuantumX and catman®Script in the Aescher tunnel in Switzerland

The monitoring of structures makes an important contribution to their reliability.

Tunnel monitoring with QuantumX and catman®Script in the Aescher tunnel in Switzerland

The monitoring of structures makes an important contribution to their reliability.

When the earth rocks... vibrating table tests at ZAG

The ZAG Ljubljana, Zavod za gradbeni tvo Slovenije, is Slovenia’s national Institute for building and civil engineering, where building products are tested and certified.

More safety in buildings: Experimental stress analysis of a passive reinforcement anchorage

An important aspect when designing concrete structures is the precise measurement of anchorage lengths, particularly when

they are positioned in corbels, cornices or load-bearing areas. The connection conditions are...