reports in applied measurement

reports in applied measurement is an in-depth journal on measurement technology comprising articles submitted by independent authors.

RAM has a tradition going back to the mid-1960s.

It is edited by Dr. Martin Stockmann from the Institute of Mechanics at the University of Chemnitz, Germany. It is issued twice yearly in English and German exclusively on our website.

Metrological recording of deformation development in ultra-high performance concrete (UHPC) in a triaxial test cell

This article shows that by using a "triaxial cell" test rig, it is possible to determine the triaxial strengths for both static and dynamic loadings.

Numerical simulation of strain gages

This article describes how to apply numerical methods to determine the properties of the strain gages and then, by specifically modifying the material and geometric properties, to change the strain gages so that they meet certain...

Monitoring the Reichenbach and Albrechtsgraben viaducts

Normally, road bridges are visually inspected at regular intervals, in order to detect any defects and/or to decide whether additional rehabilitation might become necessary.

Identifying the material parameters of carbon fiber reinforced plastics with strain gages, taking transverse sensitivity into account

This article describes the process of identifying the material parameters of characteristic carbon fiber reinforced plastics (CRP).

reports in applied measurement


ISSN 1614-9912