Industrial Amplifiers - Software and Firmware Downloads

Veuillez entrer votre adresse email

Si vous avez déjà un compte sur HBM.com, entrez ici votre adresse email pour obtenir l'accès illimité à la totalité des documentations techniques HBM.

PMX

Title

Description

Date

Version

Size

Related Documents

The driver allows to integrate QuantumX, SomatXR, PMX and MGCplus in LabVIEW.
Please see the Release Notes for futher details and requirements.

07/2015 2.0.2 8 MB Release Notes

PMX device description file for Ethernet/IP.

02/2015 0.24 62 KB

This project is a macro-project and contains CAE data for Eplan Electric P8.

12/2013 2.00 27 MB

PMX device description files for ProfiNet RT and IRT.

02/2015 2.3 84 KB

Archive including all current files for CodeysV3.5SP3 software installation and PMX-Package.

Included are also PMX Codesys examples for an easy Startproject, Codesys-WebVisualisation,

PMX-CAN-interface support for CAN-devices(e.g.SomatCR) and CAN-Master-Slave communication.

The examples do not imply any warranty or guarantee.

01/2014 1.02 439 MB Release Notes

This is a collection of Codesys software achives for typical requirements around PMX.

They show a step-by-step solution up to the running project in Codesys and PMX.

Available languages: german, english.

     

  • PMX Web-visualisation
  • PMX in CAN-Master and -Slave mode
  • PMX with CAN-modules for temperature and climate measurements
  • PMX with Client-Server communication via TCP/IP
  • PMX with integrated data-storage on internal memory or USB-stick

 

Legal notice: The examples given are intended to illustrate the solution and integration into PMX.

The examples do not imply any warranty or guarantee.

02/2015 1.0 69 MB

This example considers a simple test assembly including a AlanBradley PLC Compact Logix L24ER and a PMX.

In this example, consistent (coherent) data are written and read via the Ethernet/IP.

Legal notice: The example given is intended to illustrate the integration of PMX into AlanBradley's software RSLogix 5000 via Ethernet/IP.

This example does not imply any warranty or guarantee.

04/2014 2 MB

This example considers a simple test assembly including a Beckhoff PLC CX1020 and a PMX. In this example, consistent (coherent) data are written and read via the EtherCat and shown is a visualization panel. Legal notice: The example given is intended to illustrate the integration of PMX into Beckhoff TwinCat software via EtherCat. This example does not imply any warranty or guarantee.

04/2014 1 MB

This example considers a simple test assembly including a Siemens CPU315-2 PN DP and a PMX.

In this example, consistent (coherent) data are written and read via the Profinet.

Legal notice: The example given is intended to illustrate the integration of PMX into Siemens' Step7 software via Profinet.

This example does not imply any warranty or guarantee.

04/2014 2 MB

This example uses the internal PMX command-set and illustrates how to connect, read, write, measure with PMX.

Requirements: LabView 2011

It has a linewriter included and can sent/receive single commands to/from PMX.

All commands are described in the PMX manual.

This example does not imply any warranty or guarantee.

LabVIEW is a registered trademark of National Instruments Corporation.

02/2015 1.1 543 KB Release Notes

This example uses the internal PMX command-set and illustrates how to connect, read, write, measure with PMX.

Requirements: LabView 2012

It has a linewriter included and can sent/receive single commands to/from PMX.

All commands are described in the PMX manual.

This example does not imply any warranty or guarantee.

LabVIEW is a registered trademark of National Instruments Corporation.

02/2015 1.1 541 KB Release Notes

This is a collection of technical application reports for typical requirements around PMX.
They show a step-by-step solution up to the running project in PMX.
Available languages: german, English and French.

  • PMX with Codesys and Codesys WebVisualisation
  • PMX as CANmaster and CANslave (read/write CAN messages)
  • PMX with IEPE-sensors, T40 torque-sensors, Piezoelectrical-sensors
  • Read sensor signals via CAN, e.g. torque/speed (T12), temperature, climate
  • PMX with calculated channels:

    • Event-counter, X-borders, tolerance-band, tolerance-windows, result-force
    • Mechanical work, stress-analysis
    • Combined Triggeroutput
    • 6x6 Matrix-compensation (noise reduction for Multi-Component sensors)
    • PID-regulator, PT100-measurement

  • PMX integration in a PC-network (Windows or Linux)

    • Using the PMX dotNET-API
    • Using the PMX command-set under LabView
    • Using PMX together with catman for DAQ

  • PMX integration in an automation-network

    • EtherCat and TwinCAT(Beckhoff)
    • ProfiNet (Isonchronus-Real-Time (IRT) and Simatic-manager (TIA-portal, Siemens)
    • Ethernet/IP and RSLogix (Rockwell Automation)

  • PMX NTP-synchronisation with QuantumX
  • PMX with internal Dats-Storage or on USB-Stick

Legal notice: The examples given are intended to illustrate the solution and integration into PMX.
The examples do not imply any warranty or guarantee.

04/2015 1.2 62 MB

Archive including all current files for firmware and PMX WebServer.

To update firmware and WebServer the existing WebServer in the PMX

can be used (no additional software or hardware needed).

09/2015 2.04 33 MB Release Notes

This project is a 3D-modell as STEP-files for CAE

12/2012 4 MB

PMX device description file for EtherCat.

02/2015 1.3 58 KB

The HBM common API enables users to develop their own PC software application using Microsoft Visual Studio, to integrate HBM DAQ systems QuantumX, SomatXR, PMX and MGCplus.
The download includes the API as well as documentation and examples.

12/2015 3.0 12 MB

Only available in German language.

The driver allows to integrate QuantumX, SomatXR, PMX and MGCplus in DIAdem.

Please see the Release Notes for further details and requirements.

01/2016 6.0 52 MB

PME Series (including MP85A)

Title

Description

Date

Version

Size

Related Documents

For PME hardware version 1.xx (MP01-MP70) and all MP85/DP! For newer devices, please use the PME firmware for hardware version 2.xx on this page. Archive including all current firmware files for modules of the PME series. The appropriate firmware loader is part of the PME assistant. The zip file has to be extracted into the PME assistant directory. It includes following firmware versions:

  • MP01 Version 1.12
  • MP30 Version 1.04
  • MP30DP Version 1.04
  • MP55 Version 1.42
  • MP55DP Version 1.42
  • MP55DPS6 Version 1.42
  • MP60 Version 1.18
  • MP60DP Version 1.18
  • MP70DP Version 1.05
  • MP70DPS7 Version 1.05
  • MP70S7 Version 1.05
  • MP85 Version 1.10
  • MP85DP Version 1.10
05/2007 HW1 887 KB

This project is a macro-project and contains CAE data for Eplan Electric P8.

08/2011 1.00 19 MB

For PME hardware version 2.xx (MP01-MP70) and all MP85A/ADP! For older devices, please use the PME firmware for hardware version 1.xx on this page. Archive including all current firmware files for modules of the PME series. The appropriate firmware loader is part of the PME assistant. The zip file has to be extracted into the PME assistant directory. It includes following firmware versions:

  • MP01 Version 2.00
  • MP30 Version 2.02
  • MP30DP Version 2.02
  • MP55 Version 2.06
  • MP55DP Version 2.06
  • MP55DPS6 Version 2.02
  • MP60 Version 2.00
  • MP60DP Version 2.00
  • MP70DP Version 2.00
  • MP70DPS7 Version 2.00
  • MP70S7 Version 2.00
  • MP85A Version 2.36
  • MP85ADP Version 2.36
  • MP85A-S Version 2.36
  • MP85ADP-S Version 2.36

07/2013 HW2 2 MB Release Notes

PME assistant, firmware loader and USB driver (for Windows XP, Windows Vista and Windows 7/8) for comfortable setup and visualisation. For smooth operation of modules with CAN interfaces, use the PEAK USB-to-CAN dongle. All required drivers are included and will be installed during startup.

This download includes:

  • PME-Assistant (V3.4.206)
  • PME-Firmware Loader (V1.1.7)
  • IPM data conversion (V1.1)

... and the demo versions of:

  • EASYteach (V1.0.5.10)
  • MP85A-Toolkit (V1.0.5.12)
  • EASYmonitor CE (V1.1.1.1)
  • INDUSTRYmonitor (V1.2.1.10)

You can start those demo versions up to 25 times for free. To buy the full licence please visit the HBM shop or ask your local HBM representative.

07/2015 1.50 163 MB Release notes

EDS files for PME (MP01, MP30, MP55, MP60, MP85).

11/2011 1.01 33 KB

PROFIBUS DP master file for PME: (MP30DP, MP55DP, MP60DP, MP70DP, MP70DPS7,MP85MP). German version: GSD file, English version: GSE file.

07/2013 1.20 30 KB

This project is a macro-project and contains CAE data for Eplan Electric P8.

08/2011 30 MB

The basic sequence of transmission of measured value (Float data format) from the MP85ADP curve memory via the Profibus-DP interface to a master (e.g. Siemens PLC) is shown in this file.

07/2015 926 KB

Program example to the communication of the HBM process-controller MP85 with a Siemens Siemens CPU317-2 DP:
The example of the communication with the MP85A about Ethernet please unzip recursive in the ZIP archive (relatively stored paths). The program sends and receives data by means of the functions AG_send and AG_Recv (FC5 and FC6). It are sent 10 bytes to the SPS and 14 bytes should be received again. In this project the Siemens CPU317-2 DP has the IP address 172.21.64.250. The IP address of the MP85 is 172.21.64.253 (port 4020). A description with program-code and comments is shown in the documents „OP1_MP85A_Eth-Com-CPU317-2 DP.pdf “
Legal notice: The example given is intended to illustrate the integration of the MP85ADP(-S) into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.

07/2015 2 MB

Example-Sequence to read and write consitent data as well an example to read and write the workpiece-id via Profibus-DPV1 with Siematic Step7:
This basic example shows the transmission of measuring-value and Control-word (Float data format) from the MP85ADP(-S) via Provibus-DP interface to a master (e.g. Siemens PLC). Programming is done in Step7 Siemens software using the function blocks for reading (SFC14) and writing (SFC15) MP85ADP data. Further more the example contains reading and writing the workpiece-id via the Profibus DPV1-function using the function-blocks for reading (SFB52) und writing (SFB53) to MP85ADP(-S). A description with program-code and comments is shown in the documents „OB1_DPV1_Werkstueck_de.pdf“ and „OB1_DPV1_Werkstueck_en.pdf“.
Legal notice: The example given is intended to illustrate the integration of the MP85ADP(-S) into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.

07/2010 6 MB

digiCLIP

Title

Description

Date

Version

Size

Related Documents

EDS files for digiCLIP DF30DN and DF31DN.

05/2015 1.12 25 KB

Contains the installation of the DeviceDTM in German and English for Windows 2000/XP/Vista/Windows7/Windows8 operating systems.

Prerequisite for using digiCLIP DTM setup is the installation of a frame application (e.g. FDT container, PACTware) - not included in this download.

12/2010 1.2.0.166 13 MB Release Notes

GSE/GSD files for digiCLIP DF30DP and DF31DP.

12/2012 1.34 3 KB

This project is a macro-project and contains CAE data for Eplan Electric P8.

08/2011 1.00 42 MB

EDS files for digiCLIP DF30CAN and DF31CAN.

06/2014 1.36 / 1.20 13 KB

This applicatin is to describe an example of a small-scale digiCLIP amplifier application in a CAN network using a CANopen based PLC. In this application, load cells implemented as strain gage full bridges are used for determining the filling level in a tank and taring it to 0 ... 100% using a PLC connected to the digiCLIP. This example does not imply any warranty or guarantee.

07/2015 1 MB

The CX-Integrator example program shows the basic test setup of a digiCLIP DF31DN connected to an Omron Sysmac CJ1M SPS with a CS1/CJ1 DRM21 fieldbus controller. In this example, consistent (coherent) data is read and written over the DeviceNet. The DF30DN operating manual provides all possible commands and values. This example does not imply any warranty or guarantee.

07/2015 763 KB

This example considers a simple test assembly including a Siemens CPU313-2DP and a DF30DP/DF31DP (digiclip). In this example, consistent (coherent) data are written and read via the Profibus with SFC14 and SFC15. As an additonal programming the parametercontainer is programmed to configure the DF30DP in the cyclic data exchange. To read configurations with DPV1 the Siemens function block SFB52 (PNO AK1131)is programmed, too. All commands and values for the configuration are shown in the official manual.

Legal notice: The example given is intended to illustrate the integration of the DF30DP into Siemens' Step7 software via Profibus. This example does not imply any warranty or guarantee.

07/2015 7 MB

Archive including all current firmware files for modules of the digiCLIP series. The appropriate firmware loader is part of the digiCLIP assistant. The zip file has to be extracted into the digiCLIP assistant download directory.

DF30CAN version 1.44
DF31CAN version 1.28

DF30DP version 1.42
DF31DP version 1.28

DF30DN version 1.12
DF31DN version 1.12

05/2015 555 KB Release Notes

digiCLIP Assistant, Firmware Loader and USB Driver (for Windows XP, Windows Vista and Windows 7/8) for easy setup of digiCLIP modules and for visualization.

For smooth operation of modules with CAN and DeviceNet interfaces, use the PEAK USB-to-CAN dongle.

For Profibus operation Hilscher and Siemens CP5511/12 and CP5711 is supported - to handle digiCLIP firmware-updates via CP5711 digiCLIP-modules have to be equipped with a adapted bootloader which is implemented starting with following serial-numbers: (DF30DP: 816711801 / DF31DP: 817427801).

All required drivers are included and will be installed during startup.

05/2015 2.6.2 39 MB Release Notes

Clip

Title

Description

Date

Version

Size

Related Documents

This project is a macro-project and contains CAE data for Eplan Electric P8.

03/2012 1.00 17 MB

MGA II

Title

Description

Date

Version

Size

Related Documents

This project is a macro-project and contains CAE data for Eplan Electric P8.

03/2012 1.00 19 MB

PACEline CMD

Title

Description

Date

Version

Size

Related Documents

Archive including all current firmware for all modules of the CMD series (CMD600 and CMD2000).
Please use "CMD Firmware Updater for Version 3.62 and higher" on this page.

05/2015 3.69 247 KB Release Notes

Start the Setup-file and follow the instructions.

12/2013 1.00 2 MB Release Notes

This project is a macro-project and contains CAE data for Eplan Electric P8.

10/2011 1.00 18 MB

This Siemens Step7 example describes a project to connect the type CMD measuring amplifier from HBM GmbH to a Siemens S7-315-2 PN/DP CPU via UDP and store the measured values transmitted via UDP in a data module. The measured values are to be read and processed with up to 1000 Hz via UDP.

HBM does not guarantee the completeness and correctness of this example.

08/2011 3 MB

CMD Assistant for Windows 2000, XP, Vista, Windows 7 and Windows 8. Allows the easy setup of CMD modules, visualization and process-data storage. All required drivers are included and will be installed during startup.

Starting with assistant-version 1.2.4.0 only CMD with firmware 3.0 and higer can be used. Devices with firmware 2.9 and lower are shown in the device-scan but marked red with a note for firmware-update. Please do also a firmware-update for those devices, for features see release-notes.

11/2011 1.2.6.0 79 MB Release notes

To simplify the use of CMD meauring amplifier a complete support for communication in form of a Labview driver is available, respectively Labview programs/subroutines called virtual instruments (VIs).
The purpose of this document is to explain in detail all aspects of the Labview CMD driver:

     

  • Driver structure
  • VI blocks
  • Application example – getting started
  •  

The CMD driver is completely written in Labview Professional Development System. In order to use the drivers the user will need Labview version 9.0.1 or later.
This example does not imply any warranty or guarantee.

07/2015 3 MB

Copy all files in one folder and start the file CMD600_Updater.exe

07/2014 1.00 407 KB

MVD and MVD SCOUT55

Title

Description

Date

Version

Size

Related Documents

This project is a macro-project and contains CAE data for Eplan Electric P8.

03/2012 1.00 19 MB

System-CD for MVD and MVD SCOUT55 modules.

09/2008 2.2 40 MB

TEDSdongle

Title

Description

Date

Version

Size

Related Documents

Conversion template containing the IEEE codes for TEDS of all HBM transducers.

12/2013 2 KB

TEDSdongle Setup

01/2013 3.4.0.6 33 MB
Contactez-nous Nous sommes à votre écoute pour répondre à toutes vos demandes.