Ballistics & Missile Testing: Making Sure it is Recorded the First Time
With once in a lifetime tests, you want to make certain that you capture the event. Genesis HighSpeed by HBM has the tools and experience to do just that. For over 35 years, Genesis HighSpeed has been a market leader in high resolution, and high speed transient capture.
With our line of rugged hardware, mixed with intuitive software, we make certain that you capture that data from a test that cannot be repeated.
Blast Hazard Assessment
It is important to know the power and duration of an explosive event in order to determine the possible effect on personnel in the vicinity. These effects may have to be known in order to protect soldiers under attack or for those operating weapons. Knowing this information will allow planning for how close one can be to explosions or how often a weapon can be fired without causing damage to the operator.
The GEN5i data acquisition system with our Perception software has the ideal performance characteristics to allow for the recording of this type of test. Sensitive microphone pickups can be used to calculate blast duration and strength. Using automated routines, a report can be quickly and automatically generated.
Other Applications
Our Liberty systems are also used in a variety of other test applications, from launch platform testing through battlefield deployment of munitions. By measuring strain, acceleration, blast patterns, pressure waves and detonation times just to name a few, can provide the complete data acquisition solution.