Marine Industry

Solutions HBM pour la marine et la construction navale

Depuis des milliers d’années, la marine a toujours été l’âme même du commerce international. La demande croissante pour une plus grande efficacité, les nouvelles directives sur les émissions de gaz de plus en plus rigoureuses et les nouveaux systèmes de propulsion des bateaux apportent de nouveaux défis dans la construction navale à travers le monde.

HBM propose la meilleure solution qui soit adaptée et orientée vers l’avenir, pour vous assurer le développement et la production des bateaux, des moteurs marins et autres composants maritimes.

Par exemple, dans les applications suivantes :

Essais de moteurs à combustion de bateaux

Testing of ship engines

Testing of ship combustion engines

This is a standard application in engine testing, however it is often still performed by means of lever arms and force transducers – thus not meeting new requirements for measurement uncertainty budgets.

Standard HBM T10FH or T40FM torque transducers are perfect for the implementation into systems for testing of ship engines. With this well accepted technology, measurement uncertainty budgets of less than 1% for the complete test systems can be met.

See also our white paper on torque measurement of ship engines

Torque transducers from HBM for ship engine testing:

T10FH analog high capacity torque flange

T40FM digital high capacity torque flange

Surveillance des moteurs à gaz avec système d'entraînement direct

Monitoring of gas engines in direct drive propulsions

Mounting of a torque flange in a drive train. (Top-right corner) Torque flange with a nominal (rated) measuring range of 2MNm.

The latest international regulations, such as MARPOL annex VI, requires significant emission reductions.

An option for this is to increase the use of gas engines, instead of classic diesel engines. Gas engines burn very cleanly therefore exhaust gas cleaning is not necessary, however to do this they need to be carefully controlled by a high precision load signal.

Torque transducers directly installed on-board of ships with gas engines (or dual fuel engines), with direct drive propulsions, can automatically optimise the gas engine performance – this also guarantees the protection of the gas engine from knocking, misfiring and overload. Furthermore, this torque flange technology has been identified and is now promoted by international marine societies.

A customized version of HBM's T10FH high capacity torque transducer is now available with ATEX certification.

T10FH torque transducer with ATEX certificate for monitoring of gas engines

Modernisation des dynamomètres hydrauliques de grande capacité

Upgrading of high-capacity hydraulic dynamometers

High capacity dynamometers are integral part of test systems for marine engines. They are often still equipped with lever arms and force transducers; however this installation limits the measurement uncertainty.

A state of the art solution is offered by HBM: installation of a torque flange directly to the output shaft of the dynamometer is by far the more precise method of doing this.

Essais de coques de navire

Que ce soit à bord du navire, sur un banc d'essai ou sur une maquette en test : l’équipement de mesure HBM permet d’optimiser les essais et la surveillance des coques des bateaux.

Utilisez la chaîne de mesure complète d'un seul fournisseur : Jauges de contrainte, capteurs, systèmes d’acquisition de données et logiciel de mesure.

A lire : Comment Qinetiq surveille la coque de son dernier catamaran à coussin d’air

Acquisition dans les simulations et essais en construction navale

Les bateaux sont parfois soumis à d’énormes contraintes mécaniques. Par conséquent, des études et des expériences sur des maquettes de navires sont réalisées dans des installations d’essais spéciales pour permettre une meilleure compréhension des phénomènes physiques de manière à optimiser la conception des bateaux.

Avoir un système d’acquisition de données puissant est une nécessité.
Les principaux instituts de recherche, par exemple l’institut MARINTEK Norway font entièrement confiance dans les systèmes d’acquisition de données HBM

Pour en savoir plus sur les systèmes d’acquisition de données HBM

Analyse structurale avec de nombreuses voies de mesure

catman®Enterprise Software

Vous souhaiter soumettre de grandes structures, par exemple un bateau, à une analyse structurale et à des essais de fatigue ! Le système d’acquisition de données MGCplus en liaison avec le logiciel catman®Enterprise est vraiment la solution idéale pour vos campagnes de mesure impliquant un nombre élevé de voies de mesure.

Plus d’information sur catman®Enterprise…

Essais de fatigue virtuels avec le logiciel nCode

nCode Fatigue and Durability Software

Les solutions logicielles nCode de HBM vous aident à comprendre les facteurs d’influence qui affectent la longévité d’un produit. Les logiciels d’essais de fatigue et de durabilité de HBM nCode vous permettent, par exemple :

  • De faire rapidement et efficacement des analyses puissantes
  • De gagner très nettement du temps en analyse – très souvent des minutes voire des jours
  • D’éviter une conception surdimensionnée entraînant des surcoûts et du poids en plus
  • D’automatiser les analyses et les processus complexes
  • De facilement partager et d’analyser les données entre services.

Voir les solutions logicielles nCode de HBM…

Pesage des bateaux, passerelles des navires et autres composants

Connaître correctement le poids du bateau est d’une importance capitale: Les capteurs de pesage HBM sont intégrés dans différents types de balance et vous assurent des résultats précis. Ils sont également livrables dans des modules de pesage, de manière à s’intégrer facilement et rapidement dans l’installation, par exemple pour le pesage de silos.

Découvrez ici « Comment un chariot de pesage anglais pèse les bateaux en utilisant les capteurs de pesage HBM

Exemples d'application dans l'industrie navale

Le projet d’explosions sous-marines, mené dans un environnement sensible sur le fleuve Columbia, respecte des limites rigoureuses de sécurité grâce à l'équipement de mesure Genesis de HBM

Deux entrepreneurs américains : Contract Drilling & Blasting et Aimone-Martin Associates, ont utilisé le système rapide d’acquisition de données GEN7t de la famille Genesis de HBM pour surveiller avec succès des explosions...

L'eDAQ de HBM surveille la coque pour un parfait succès militaire

La dernière péniche de débarquement rapide de l’armée britannique a été développée et construit par la société QinetiQ avec le système d’acquisition de données eDAQ de HBM utilisé comme moyen d’essais et système d’analyse. Le...

On lui a donné des ailes : le voilier le plus rapide du monde muni de la technique de mesure d’HBM

Quiconque souhaite faire « voler » son bateau sur les mers a besoin de matériaux et de constructions innovants. Dans le cadre du développement de son trimaran, l’« Hydroptère », Alain Thébault mise sur la technique de mesure de...

Quatre fois quatre – Pesons numériques HBM pour un chariot de pesage roulant

La société Westco Ltd., située dans le sud-ouest de l’ Angleterre, a un très grand succès dans le pesage.

Journées "Jauges de contrainte" et "DAQ" sur HBM On Tour

Profitez de notre expertise sur "l’Utilisation des jauges de contrainte" et "l'Acquisition de données" en participant aux journées gratuites HBM On Tour organisées

le 11 et 12 juin 2013 à Nantes.

Records de vitesse...

Le voilier le plus rapide au monde avec les instruement de mesure HBM.

Pour en savoir plus...

See HBM's solution for high capacity torque measurements...

SMM Shipbuilding Marine Technology Fair in Hamburg