Weight control of the metal dosage in die-casting
This article describes the design of a dosage controller which includes measurement of the level of liquid metal in the furnace.
Die-casting is a very effective way of mass-producing cast metal parts and the method is widely used in the automobile industry. Liquid metal is passed from a furnace to a casting machine where it is formed in a mold under pressure. It is important that the correct quantity of material is used as this directly affects the product quality, but there are a number of variables influencing the dosage which must be automatically controlled.
This article describes the design of a dosage controller which includes measurement of the level of liquid metal in the furnace. The level is obtained indirectly by weighing the furnace and its contents using HBM weighing equipment.
Auteur : Hans-Peter Braunger, Rudolf Hann