Metrological analysis of stresses in a recycling machine for separating materials
Because of the constantly increasing pressure on our environment caused by solid waste and contaminants and the associated negative effect on our living conditions, the problems of technical pollution control are becoming ever more important.
Because of the constantly increasing pressure on our environment caused by solid waste and contaminants and the associated negative effect on our living conditions, the problems of technical pollution control are becoming ever more important. It is clearly a matter of urgent necessity to develop ecological as well as economically sensible recycling concepts.
More than enough reference documentation is available for existing disintegrator units such as shredders, ball mills, hammer mills, impact crushers, percussion grinders, granulators, rasps and screw crushers.
Auteur : Mike Winkler