Experimental analysis of mechanical stress in passive reinforcement anchorages in C-C-T nodes
The article presents a new test for analyzing the mechanical stress of adhesion anchors in C-C-T nodes.
The article presents a new test for analyzing the mechanical stress of adhesion anchors in C-C-T nodes. The primary aim of the investigation is to develop a practical design standard which, in the form of a dimensioning program, can be used to defi ne important parameters for reinforcement anchorages. As well as the various concrete qualities and bar diameters, the parameters used in the program include the adhesion length and the angle of inclination of the tie bar.
Auteur : C. Castro, P. Miguel, M. A. Fernández, J. R. Martí
Fichiers: