Torque measurement on a single cylinder engine test bench with an HBM measurement flange
Dynamic torque measurements on singlecylinder engine test benches are now on the agenda in most of the research and development units of automotive manufacturers and suppliers.
Dynamic torque measurements on singlecylinder engine test benches are now on the agenda in most of the research and development units of automotive manufacturers and suppliers. The effect of the combustion run, the mixture formation or the internal cylinder pressure for different cylinder geometries and the various fuel injection strategies, for example, are examined in order to optimize the engines on the test bench.
Auteur : Florian Rauscher
Fichiers: