© rc10de / photocase.com

Download archive for Genesis HighSpeed software and firmware

This archive contains older and unsupported Genesis HighSpeed software and firmware.

For the latest Genesis HighSpeed software and firmware, please click here.

Description Version Build Taille Date
Dimension4i Firmware
2.10 9245 63 MByte 11/2009
GEN DAQ Series Firmware
Note: Install new GEN DAQ firmware only together with new Perception software as well.
6.12 10259 6 MByte 09/2010
GEN DAQ Series Firmware
Note: Install new GEN DAQ firmware only together with new Perception software as well.
6.12 10167 7 MByte 06/2010
GEN DAQ Series Firmware
Note: Install new GEN DAQ firmware only together with new Perception software as well.
6.12 10124 7 MByte 05/2010
GEN DAQ Series Firmware
Note: Install new GEN DAQ firmware 6.06 only together with new Perception software 6.06 as well.
6.06 9337 6 MByte 12/2009
GEN DAQ Series Firmware
Note: Install this GEN DAQ firmware 6.01 only together with Perception software 6.01 as well.
 
6.01 9076 5 MByte 03/2009
GEN DAQ Series Firmware
Note: Install new GEN DAQ firmware 6.02 only together with new Perception software 6.02 as well.
6.02 9140 6 MByte 05/2009
ISOBE5600 Firmware (archived)
2.00 12335 3 MByte 12/2012
ISOBE5600 Firmware (archived)
Firmware version 2.00.10091 for ISOBE5600
2.00 10091 2 MByte 03/2011
LIBERTY Series Firmware
Note: Install new LIBERTY firmware only together with new Perception software as well.
Note: When upgrading from 6.0x to 6.06 please also see the Information below.
6.12 10124 4 MByte 05/2010
LIBERTY Series Firmware
Note: Install new LIBERTY firmware 6.06 only together with new Perception software 6.06 as well. Note: When upgrading from 6.0x to 6.06 please also see the Information below.
6.06 10027 SP1 4 MByte 01/2010
LIBERTY Series Firmware
Note: Install new LIBERTY firmware 6.06 only together with new Perception software 6.06 as well. Note: When upgrading from 6.0x to 6.06 please also see the Information below.
6.06 9337 4 MByte 12/2009
LIBERTY Series Firmware
Note: Install this LIBERTY firmware 6.01 only together with Perception software 6.01 as well.
 
6.01 9076 4 MByte 03/2009
LIBERTY Series Firmware
Note: Install new LIBERTY firmware 6.02 only together with new Perception software 6.02 as well.
6.02 9140 4 MByte 06/2009
LIBERTY Series Firmware upgrade patch
LIBERTY Series Firmware: upgrade patch when upgrading from 6.0 through 6.04 versions to newer version.
Due to a problem in the 6.0 through 6.04 versions of firmware, you need to follow the procedure as described in the TechNote below in order to upgrade to newer version (e.g. 6.12). You also need to download the patch itself to use as described in the TechNote.
    4 MByte 05/2010
LIBERTY Series Firmware: 6.0x to 6.06 upgrade patch
Due to a problem in 6.0x firmware, you need to follow the procedure as described in the TechNote below in order to upgrade to version 6.06.
You also need to download the patch itself to use as described in the TechNote.

    4 MByte 12/2009
Patch for GN610/611 (1kV boards) DC offset in channels after changing timebase settings
The bugfix can be applied by running the installer as found in the download link above.
Please follow the instructions in the PDF linked below.
    27 MByte 01/2014
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.52 14260 252 MByte 09/2014
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.42 13287 216 MByte 10/2013
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.50 14146 249 MByte 06/2014
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.30 12335 204 MByte 12/2012
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.30 12297 204 MByte 11/2012
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.20 12083 173 MByte 03/2012
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.18 11291 147 MByte 10/2011
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.16 11067 148 MByte 03/2011
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.14 10323 141 MByte 12/2010
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.12 10124 51 MByte 05/2010
Perception FREE Viewer Software
This is the FREE viewer version of Perception software which can be downloaded and used free of charge.
6.06 9337 77 MByte 12/2009
Perception Software
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.50 14146 249 MByte 06/2014
Perception Software
Please note: From now on Perception will distinguish between uppercase and lowercase letters in the formula database (analysis). If Perception is unable to assign a channel or calculation, this is indicated by a "warning" (yellow icon). This could happen, for example, if older recordings or workbenches are loaded into the new version 6.42.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.42 13287 216 MByte 10/2013
Perception Software
Please note that Perception 6.30 contains breaking changes in the CSI and RPC interfaces. When using CSI or RPC you need to update and recompile your software before you can use it with the new version of Perception. Refer to the CSI and RPC help files for more information.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.30 12335 204 MByte 12/2012
Perception Software
Please note that Perception 6.30 contains breaking changes in the CSI and RPC interfaces. When using CSI or RPC you need to update and recompile your software before you can use it with the new version of Perception. Refer to the CSI and RPC help files for more information.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.30 12297 204 MByte 11/2012
Perception Software
Note: Perception 6.20 now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.20 12083 173 MByte 03/2012
Perception Software
Note: Perception 6.18 now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.18 11291 147 MByte 10/2011
Perception Software
Note: Perception 6.16 now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.16 11067 148 MByte 03/2011
Perception Software
Note: Perception 6.14 now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.14 10323 141 MByte 12/2010
Perception Software
Note: Install new Perception software only together with new GEN DAQ or LIBERTY firmware as well.
6.12 10124 51 MByte 05/2010
Perception Software
Note: Install new Perception software 6.06 only together with new GEN DAQ or LIBERTY firmware 6.06 as well.
6.06 9337 77 MByte 12/2009
Perception Software
Note: Install this Perception software 6.01 only together with GEN DAQ or LIBERTY firmware 6.01 as well.
 
6.01 9076 66 MByte 03/2009
Perception Software
Note: Install new Perception software 6.02 only together with new GEN DAQ or LIBERTY firmware 6.02 as well.
6.02 9140 66 MByte 05/2009
Perception Software / GEN Series firmware patch for Fiber Channels
Patch to fix a problem with fiberoptic receiver modules not starting up properly. All firmware versions up to 6.20 are potentially affected.
6.20 12163 24 MByte 08/2012
Perception Software 32-bit
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.52 14260 252 MByte 09/2014
Perception Software 64-bit
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.52 14260 256 MByte 09/2014
Perception Software 64-bit
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.50 14146 253 MByte 06/2014
Perception Software 64-bit
Please note: From now on Perception will distinguish between uppercase and lowercase letters in the formula database (analysis). If Perception is unable to assign a channel or calculation, this is indicated by a "warning" (yellow icon). This could happen, for example, if older recordings or workbenches are loaded into the new version 6.42.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.42 13287 217 MByte 10/2013
Perception Software 64-bit
Please note that Perception 6.30 contains breaking changes in the CSI and RPC interfaces. When using CSI or RPC you need to update and recompile your software before you can use it with the new version of Perception. Refer to the CSI and RPC help files for more information.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.30 12335 205 MByte 12/2012
Perception Software 64-bit
Please note that Perception 6.30 contains breaking changes in the CSI and RPC interfaces. When using CSI or RPC you need to update and recompile your software before you can use it with the new version of Perception. Refer to the CSI and RPC help files for more information.
Please also note: Perception now includes the instruments firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.30 12297 205 MByte 11/2012
Perception Software 64-bit
Note: Perception Enterprise 6.20 includes the instrument firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.20 12083 172 MByte 03/2012
Perception Software 64-bit
Note: Perception Enterprise 6.18 includes the instrument firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.18 11291 147 MByte 10/2011
Perception Software 64-bit
Note: Perception Enterprise 6.16 includes the instrument firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.16 11067 148 MByte 03/2011
Perception Software 64-bit
Note: Perception Enterprise 6.14 includes the instrument firmware. That means it no longer requires an additional download of the firmware for the GEN DAQ systems and LIBERTY.
6.14 10323 141 MByte 12/2010
Perception Software 64-bit
Note: Install new Perception 64-bit software only together with new GEN DAQ or LIBERTY firmware as well. Please make sure to install firmware upgrader first before installing Perception x64.
6.12 10124 51 MByte 05/2010
Perception Software 64-bit
Note: Install new Perception 64-bit software 6.06 only together with new GEN DAQ or LIBERTY firmware 6.06 as well.
6.06 9337 77 MByte 12/2009
Perception Software 64-bit
Note: Install this Perception 64-bit software 6.01 only together with GEN DAQ or LIBERTY firmware 6.01 as well.
 
6.01 9076 67 MByte 03/2009
Perception Software 64-bit
Note: Install new Perception 64-bit software 6.02 only together with new GEN DAQ or LIBERTY firmware 6.02 as well.
6.02 9140 67 MByte 05/2009
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.52 14260 5 MByte 09/2014
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.50 14146 5 MByte 06/2014
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.42 13287 5 MByte 10/2013
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.30 12335 5 MByte 12/2012
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.30 12297 5 MByte 11/2012
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.20 12083 5 MByte 03/2012
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.18 11291 5 MByte 10/2011
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.16 11067 5 MByte 03/2011
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.14 10323 5 MByte 12/2010
PNRF Reader Toolkit 32/64-bit
Software programming tool to read the proprietary PNRF (Perception Native Recording File) file format.
 
6.12 10124 4 MByte 05/2010
PNRF Reader Toolkit 32/64-bit
 
6.06 9337 4 MByte 12/2009
PNRF Reader Toolkit 32/64-bit
 
6.01 9076 4 MByte 03/2009
PNRF Reader Toolkit 32/64-bit
 
6.02 9140 4 MByte 07/2009