Software Downloads
Downloads for Perception and Genesis HighSpeed
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
Perception Software 64-bit | Perception 8.50 This is a major release of Perception. Due to the fixes in Perception 8.52, please download Perception 8.52 instead of Perception 8.50. New Features: • Continuous Output • RTFDB processing on CAN signal • Harmonic Analysis Display Improvements • Change from relative addressing to absolute addressing NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup. | 07/2023 | 8.50.23184 | 665 MB | Release Notes |
Perception Software 64-bit | Perception 8.60 This is a major release of Perception. Fixes:: Averaging in Spectral Display always Peak hold average In the Perception Spectral display, the averaging was always peak-hold rather than the selected linear or exponential. This issue is fixed such that now the proper averaging is done. Fundamental calculation issue on RT-FDB A problem with cross-board cycle signals used for doing fundamental calculations was solved. Change of conditional Start/Stop time does not work during the recording In Perception it is possible to conditionally start or stop a recording. Up until now it was possible to change the conditions during a recording which might lead to unexpected or undefined situations. In this release it is no longer possible to change conditions during a recording such that the conditions are always well-defined. Graphical problem in Report sheet tables in Perception A problem with columns width when automatically generating a report was solved. User defined display color is not permanent stored User-defined colors are now stored as part of the PC settings. Switching display mode to ReviewSweep does show the full recording instead sweep A problem with switching between Review and ReviewSweep in the time display was solved. Using macro function auto scale active display y-axis is takes only action on first page of the display The macro function auto scale active display y-axis now works on all pages of a display. The format of the displayed value in a marker does not reflect the format set in Properties for the marker A small formatting discrepancy between marker field and the properties of a marker was solved. Suppress overrange drawing does not work as expected Some related issues concerning drawing or suppressing overrange data where solved. Trace marker not connected to trace line A trace marker is now always connected to a trace. Load Settings menu option doesn't load workbench settings completely A problem with incomplete loading of working bench settings was solved. Apply a Thermocouple type C sensor, Perception shows type B A thermocouple type C sensor is now shown as such. Redo an existing Experiment and load existing Experiment data does not include data On opening Perception and selecting 'Redo an existing experiment and load existing experiment data', the data was not always loaded. This problem is solved. Recordings got locked up by Perception When a recording is finished, it is unlocked and can be accessed by other software. Sometimes the recording was not unlocked and this problem is now solved.
No MDF4 file when exporting using automated processing The problem of a missing MDF4 file when exporting using automated processing was solved. Sluggish behavior when loading a virtual workbench In some case, Perception could react in a sluggish manner when loading a virtual workbench. This problem is solved.
NEW Features: Add hardware settings to a recording stored on a mainframe Up until now, when a recording was made by storing all the data directly on the internal disk of each mainframe (as opposed to storing all or some of the data on PC), the hardware settings of each mainframe were not available in the recording. In the new release, it is possible to include the hardware settings of a mainframe in the recording written to the mainframe's internal disk, in order to know exactly how a recording was made. Automatic merge of mainframe data In the GHS/Perception system, it is possible, and sometimes necessary, to store a recording partially or completely on the internal disc of a GHS mainframe. In this release it has been made possible to automatically merge the different parts of a recording into a single recording file on a PC. An additional improvement in this context is that the speed of transferring a recording from a mainframe to the PC was increased by a factor 2. Rework of the Spectral Display including new features such as:
In the Measurement Uncertainty sheet, support for new hardware was added The measurement uncertainty (MU) of a measurement depends on the properties of the used hardware (sensors, acquisition cards, etc.) which should be incorporated in the MU calculations. In the Measurement Uncertainty sheet, support was added for the T12 w-version torque sensor (but not yet for the minimal torque value of 100Nm). Furthermore, support for the GN610B/GN611B acquisition card was added, as well as support for burden resistors to allow for measuring both voltages and currents with those cards. Allow publishing any value on the fieldbuses in case of an invalid signal Since not all external systems can easily handle NaN, it is now possible to select a user-defined value to publish when a signal is not valid. Allow triggering of signals in Live display based on cycles: In the Live display in Perception, signals are often not stable but 'running', just like in an oscilloscope that is not triggered. In the new release, it is possible to trigger signals based on cycle signals. Periodic signals related to a selected cycle signal will then be stable in the Live display. NEW ePower Suite Features:: Using field bus signals, allow easy detection if a setup is in steady-state A setpoint of an eDrive setup (e.g., the efficiency for a certain torque/speed combination), is commonly measured when a system is in steady-state. In the new release, additional RTFDB functions can be instantiated by the ePower suite which, for a number of relevant signals, determine the mean and standard deviation. The user can determine how the samples to determine if mean and standard deviation are selected in terms of a specified number of samples or as a time interval. NEW Features for Hardware:: XCP over Ethernet This is the first major release which will support “XCP Over Ethernet” in our mainframes. This release supports the functionality of “XCP Over Ethernet – Output” which means data from the mainframe (slave) can be read by the master via XCP. In Perception, Real time data -> Publishing , a new column “Publish to XCP over Ethernet” will be available to allow publishing like existing fieldbus. For generating the A2L file, “Save A2L file as…” button is available. Known Limitations for 8.60 release:
Mainframe control via EtherCAT PDO This is the first major release which will allow mainframe control via EtherCAT PDO. On EtherCAT, several communication protocols are available. Up until now, GHS provided Remote Control via EtherCAT CoE (CAN over EtherCAT), but only SDO as the supported mechanism. From this release onwards, PDO will be supported as well. FieldBus Remote Control documentation may be referred for more information on the available commands and how to use them and return code description. Improvements in Perception :: Modernized the look-and-feel of Perception Many of the icons and graphics were updated to give a more modern look-and-feel and to improve usability. Prevent large MatLab/MDF4 export files due to asynchronous signals In the new release, when exporting signals from Perception to Matlab or MDF4, it is now possible to export asynchronous signals as asynchronous signals, or resampled at a lower user-defined sample rate leading to significantly smaller file sizes for those formats. Improve how a user can see and print the hardware settings from a recording Up until now, hardware settings of a recording could be printed by loading a recording as Active, and then selecting Settings. Two additional entries are shown in the Print sub menu to make this easier: 'Settings from active recording...' and ' Settings from current settings...' . Report CAN signal definition errors in Perception: When a wrong definition of the setup of CAN channels is provided, Perception now gives an error message such that the setup can be corrected. Add key-mouse combination for temporarily grouping of cursors: Currently the user has the option to group/ungroup cursors by pushing a button in the menu bar. To improve usability it is now possible to press the Alt-key, drag one of the cursors and the related cursors will move as a group. This works for horizontal, vertical and slope cursors. Improvements for Hardware:: Allow for unsigned/signed 16-bit CAN inputs Next to 32-bit and 64-bit signed and unsigned CAN signals, we now also allow for 16-bit signed and unsigned CAN input signals. Allow integrating asynchronous samples Up until now, the IntegrateGated() function could only handle synchronous signals to be integrated (such as instantaneous electrical power) but not asynchronous signals which are used, for example, to describe the instantaneous mechanical power. From this release, this function can also handle asynchronous signals. Additional CAN sample rates In previous releases, all CAN input signals to a GHS mainframe were sampled at a rate of 100S/s. It is now possible to choose a different sample rate for each CAN recorder. When choosing a higher sample rate, the maximum number of allowed channels is reduced. The constraint is that the sum, over all CAN recorders, of the product of the sample rate and the number of channels should be lower than 100,000. Some feasible examples are as follows:
| 01/2024 | 8.60 | 769 MB | Release Notes |
Perception Software 64-bit | Perception 8.54 This is a minor release of Perception. Due to the fixes, please download this release instead of Perception 8.52. Various stability and performance enhancements implemented, see release notes for details. NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup. | 09/2023 | 8.54.23248 | 732 MB | Release Notes |
Perception Software 64-bit | Perception 8.52 This is a minor release of Perception. Due to the fixes, please download this release instead of Perception 8.50 Fixes: No special license for RTFDB on CAN inputs: Perception 8.50 requires a special license to allow processing CAN signals in the RTFDB. This feature is free of charge for customers within Perception maintenance, so it licensing is no longer required. CAN bus stopped unexpectedly A problem is solved where the CAN bus stopped unexpectedly. New type of Peak CAN dongle was not accepted Peak provides the USB CAN dongle with different internal chip sets. The updated Peak dongles are now also recognized and can be used. NaN in log file when doing processing When using one of the FDB functions (CycleFundamental) the output may give NaN. This problem is solved. Freeze when duplicating signals for automated recording processing The system is made robust against selecting the same signal multiple times when doing automated recording post-processing. New Features: Continuous Output
RTFDB processing on CAN signal:
Since some RTFDB functions can generate triggers, this also makes it possible to generate triggers based on CAN signals. Harmonic Analysis Display Improvements:
Change from relative addressing to absolute addressing:
NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup | 07/2023 | 8.52.23198 | 727 MB | |
Perception Software 64-bit | Perception 8.28 This is an minor release of Perception mainly improving stability, fixing known problems and adding minor new features. This is not shipped out with the hardware but only available via web download. Details about fixed issues and new features can be found in the release notes. Note: Perception includes the instruments firmware for GEN DAQ systems. So there is no separate firmware available for GEN DAQ systems. When you connect to hardware using a new version of Perception, the firmware in the hardware will be upgraded accordingly to the same release level. | 07/2022 | 8.28.22200 | 602 MB | |
Perception COM-RPC | Installer of the RPC COM wrapper and RPC documentation | 09/2023 | 8.54 | 5 MB | |
Hardware Peripheral Update Package | Update HBM approved GEN DAQ hardware peripherals. For example allowing new types of (solid state) drives. | 09/2023 | 8.54.23248 | 6 MB | |
Hardware Peripheral Update Package | Update HBM approved GEN DAQ hardware peripherals. For example allowing new types of (solid state) drives. | 07/2022 | 8.28.22200 | 5 MB | |
GENDAQ API v3 | GENDAQ API v3 for Perception V7.40, V7.50 and V7.60 | 01/2019 | 6 MB | ||
GEN3i/GEN7i Update Package | The GEN3i/GEN7i Cumulative Update Package contains updated drivers for GEN DAQ “i” type mainframes. There is a version 4.1.1975 of the RTS IEEE1588 PTP driver, and the latest GEN hardware drivers needed when upgrading an older, Windows 7 based GEN3i/GEN7i to Windows 10. | 11/2018 | 8 | 130 MB | |
GEN3i/GEN7i Service Installer | Tool to extract the GEN3i/GEN7i Service from the installed version of Perception. After a fresh install of the Windows OS, the GEN3i/GEN7i service is missing and will be installed using this tool. | 12/2020 | 1 | 181 KB |
Downloads for Genesis HighSpeed Interfacing: Perception Custom Software Interface (CSI)
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
Perception CSI - Data Sheet | Perception CSI specifications | 12/2011 | 120 KB | ||
Perception CSI training - Data Sheet | Perception CSI training specifications | 12/2011 | 2 MB | ||
Perception CSI How to get started | This document describes what you need to create your own Perception CSI extensions. | 05/2019 | 65 KB | ||
CSI Examples | Examples used in the CSI Programming User Manual | 09/2020 | 6.0 | 678 KB | |
Perception Help File | Perception Programming Interfaces Help file | 05/2019 | 2019 | 21 MB | |
Perception CSI Sheet Project Template.vsix | Perception CSI Sheet template file for Visual Studio 2017 and later | 06/2022 | 5.0 | 116 KB | |
Perception.ScriptAction.Template.vsix | Perception CSI script action template file for Visual Studio 2017 and later | 06/2022 | 5.0 | 76 KB | |
Perception and GEN series: CSI Programming - User Manual | User manual Perception CSI programming | 03/2020 | 5.0 | 3 MB | |
Perception CSI 64-bit | 01/2023 | 8.40.23009 | 2 MB | ||
Perception CSI 64-bit | 05/2023 | 8.48.23109 | 2 MB |
Perception Custom Software Interface (CSI): Examples & Trial Versions
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
Perception CSI: Sensor Barcode Reader - HOTnote | Perception CSI: Sensor Barcode Reader - HOTnote | 436 KB | |||
Perception CSI: Seismic Measurement - HOTnote | Perception CSI: Seismic Measurement - HOTnote | 427 KB | |||
Word Organizer Demo Files | Demo files which can be used by the Perception Word Organizer | 11/2010 | 1.0 | 1 MB | |
Perception CSI Extension - Datasources ASCII Export - User manual | 06/2009 | 1.0 | 445 KB | ||
Harmonic Analysis Sheet- User manual | User manual Harmonic Analysis Sheet | 06/2020 | 4.0 | 2 MB | |
Time Markers Table User Manual | User manual Time Markers Sheet | 06/2011 | 1.0 | 1 MB | |
Calculator Sheet User Manual | User manual Calculator Sheet | 06/2022 | 3.0 | 916 KB | |
Word Organizer Sheet User Manual | User manual Word Organizer | 06/2022 | 2.0 | 874 KB | |
Log File Reader User Manual | User manual Log File Reader | 06/2022 | 2.0 | 1 MB | |
Perception CSI Extension - Seismic Measurement - User manual | 06/2022 | 1.1 | 1 MB | ||
Calculator Sheet Trial Version | Calculates and displays statistical information of recorded data. Alarm levels can be used to color individual calculated results | 06/2022 | 3.4 | 2 MB | |
Time Markers Table Trial Version | Shows all time markers including triggers in a table. Can be used for navigating in Perception Display to specific trigger. | 06/2022 | 2.1 | 2 MB | |
Perception CSI Harmonic Analysis Sheet Trial Version | Calculate the amplitude of the harmonic components of a periodic signal using the Fourier series. | 06/2022 | 4.1 | 11 MB | |
Log File Reader Trial version | Reading back Perception Logged data into a Perception User Table. The data can be filtered and the layout can be adjusted | 06/2022 | 2.1 | 2 MB | |
Word Organizer Sheet Trial Version | Create a new Word or PDF report by assemble existing Word documents generated during a recording. Also bitmaps or richtext files can be added | 06/2022 | 2.1 | 2 MB | |
Drop-down functions User manual | 08/2022 | 1.0 | 368 KB | ||
Perception STL Verification Sheet | Sheet works with Perception 8 or later and explains the working of the STL formulas. The sheet can be used to verify the STL calculations on user data. | 03/2023 | 3.7 | 4 MB | |
Perception CSI 64-bit | 09/2023 | 8.54.23248 | 2 MB |
Downloads for Genesis HighSpeed Interfacing: Perception Remote Control
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
Perception Remote control - Data Sheet | 265 KB | ||||
Perception remote control using LabVIEW - User Manual | 10/2012 | 1.2MB | 1 MB | ||
Perception remote control using DIAdem - User Manual | Perception RPC using DIAdem | 10/2015 | 1.0MB | 958 KB | |
Perception remote control using LabView Demo source code | LabView source code of the Perception remote control Demo | 06/2019 | 1 MB | ||
Perception remote control using LabView Demo | LabView Demo program using the Perception RPC interface | 06/2019 | 144 MB | ||
Perception COM-RPC.msi | Installer of the RPC COM wrapper and RPC documentation | 06/2019 | 7.40 | 7 MB | |
Perception Remote Control RPC Demo | Simple Perception RPC demo program | 06/2019 | 1.3.19169 | 1 MB | |
Perception Remote Control RPC Demo Source code | C# source code of the Perception RPC Demo | 06/2019 | 1.3.19169 | 617 KB | |
Perception remote control using MATLAB - User manual example files | Perception RPC using MATLAB example code | 06/2019 | 26 KB | ||
Perception RPC/COM Interfaces Helpfile | Programming Help file Perception RPC/COM interfaces | 06/2019 | 7.40 | 851 KB | |
Perception Matlab® Remote Control - User Manual | 244 KB | ||||
Perception Remote Control RPC ePower Demo Source Code | C# source code for the Perception RPC ePower demo program | 09/2020 | 2.0.20251 | 671 KB | |
Perception Remote Control RPC ePower Demo | Simple Perception RPC ePower demo program | 09/2020 | 2.0.20251 | 1 MB | |
Perception Remote Control RPC ePower Demo | Simple Perception RPC ePower demo program | 09/2022 | 2.1.22252 | 2 MB |
Downloads for Genesis HighSpeed Interfacing: PNRF Reader Toolkit
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
PNRF Reader Toolkit - User manual | PNRF Reader User manual | 07/2009 | 1.1 | 2 MB | |
PNRF Reader Toolkit- MATLAB example manual | PNRF Reader Example manual on how to read PNRF data files into MATLAB | 317 KB | |||
PNRF Reader Toolkit - Training material | PNRF Reader Training material documentation and code examples | 11/2021 | 4 MB | ||
PNRF Reader Toolkit | PNRF Reader Software installation to read the proprietary PNRF (Perception Native Recording File) file format. | 07/2022 | 8.28.22200 | 7 MB | Release Notes |
PNRF Reader Toolkit | PNRF Reader Software installation to read the proprietary PNRF (Perception Native Recording File) file format. | 07/2022 | 8.30.22203 | 7 MB | Release Notes |
Export PNRF Applic. - User Manual | 368 KB | ||||
PNRF Reader Toolkit | PNRF Reader Software installation to read the proprietary PNRF (Perception Native Recording File) file format. | 01/2023 | 8.40.23009 | 7 MB | Release Notes |
PNRF Reader Toolkit | PNRF Reader Software installation to read the proprietary PNRF (Perception Native Recording File) file format. | 05/2023 | 8.48.23109 | 7 MB | Release Notes |
PNRF Reader Toolkit | PNRF Reader Software installation to read the proprietary PNRF (Perception Native Recording File) file format. | 09/2023 | 8.54.23248 | 7 MB | Release Notes |
Downloads for Genesis HighSpeed Interfacing: GEN DAQ API
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
GEN DAQ API C source archive (*.gz format) | Archive containing examples, help file and required source code for the ‘C’ interface. | 08/2020 | 4.0 | 1 MB | |
GEN DAQ API Installer for Windows | Running the install will copy all examples, help files and source code available for the GEN DAQ API to the PC. The install contains files for both the .NET and ‘C’ interface. The files will be installed to: C:\GEN DAQ API. | 01/2023 | 5 MB | ||
GEN DAQ API Installer for Windows | Running the install will copy all examples, help files and source code available for the GEN DAQ API to the PC. The install contains files for both the .NET and ‘C’ interface. The files will be installed to: C:\GEN DAQ API. | 05/2023 | 5 MB | ||
GEN DAQ API Installer for Windows | Running the install will copy all examples, help files and source code available for the GEN DAQ API to the PC. The install contains files for both the .NET and ‘C’ interface. The files will be installed to: C:\GEN DAQ API. | 09/2023 | 8.54.23248 | 5 MB |
Downloads for Genesis HighSpeed Interfacing: EtherCAT Interface
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
GEN7tA - User Manual | 12/2016 | 2.1 | 47 MB |
Downloads for Perception: GPL Sources
主题 | 描述 | Date | Version | Size | Related Documents |
---|---|---|---|---|---|
GPL Sources GEN3t/GEN7tA/GEN17tA/GEN2tB | GPL file for GEN3t/GEN7tA/GEN17tA/GEN2tB Data Acquisition Systems | 07/2022 | 8.28.22200 | 23 MB | |
Genesis FLOSS | FLOSS (Free Libre & Open Source Software) description of the Genesis software stack | 01/2023 | 210 KB | ||
GPL Sources GEN3t/GEN7tA/GEN17tA/GEN2tB | GPL file for GEN3t/GEN7tA/GEN17tA/GEN2tB Data Acquisition Systems | 01/2023 | 8.40.23009 | 4 MB | |
GPL Sources GEN3t/GEN7tA/GEN17tA/GEN2tB | GPL file for GEN3t/GEN7tA/GEN17tA/GEN2tB Data Acquisition Systems | 05/2023 | 8.48.23109 | 4 MB | |
Genesis FLOSS | FLOSS (Free Libre & Open Source Software) description of the Genesis software stack | 05/2023 | 210 KB | ||
GPL Sources GEN3t/GEN7tA/GEN17tA/GEN2tB | GPL file for GEN3t/GEN7tA/GEN17tA/GEN2tB Data Acquisition Systems | 09/2023 | 8.54.23248 | 4 MB | |
Genesis FLOSS | FLOSS (Free Libre & Open Source Software) description of the Genesis software stack | 09/2023 | 8.54.23248 | 210 KB |