プラント製造プロセスにおける計重・計量技術
プロセス上で行われるチルドあるいは加熱工程の影響から計量器を引き離すにはどうしたらよいか?攪拌機をプロセス設備にフィットさせるにはどうしたらよいか?攪拌機がブラケット上でサポートされなければならない時は、どのような設計にしたら良いのか?
[Translate to 日本語:] Hans-Jürgen Keil Anlagenbau GmbH & Co. KG, a company based in Hunteburg, Germany, designs and constructs complete production machines for batching and mixing liquid components and solids. Mixers and reactors which accomodate quantities of up to 20 t are not uncommon in these machines.
Weighing technology in process plant engineering
These days it would be hard to imagine solutions for batching and mixing processes without involving weighing technology. This is particularly true if the characteristics of the raw materials do not allow for any other method of measurement.
However, since the batching process has to be accurate and reproducible in order to achieve optimum results from the mixing process, the questions and tasks facing designers are frequently extremely difficult to solve:
- How to uncouple a reactor that has to be chilled or heated in the course of a process?
- What should the approach be if the mixer has to be fitted with a stirrer?
- How to design the platform if the mixer has to be supported on brackets?
Keil Anlagenbau answered the questions by making use of HBM weighing technology and analysis electronics.
The right load cells for every challenge
Keil Anlagenbau chose from HBM’s extensive range of load cells and associated accessories bearing in mind the application and the ambient conditions. Their favorites include the HLC load cells with the Easy top elastomer bearing and the RTN load cells with the MLAR tank weighing module.
The right analysis electronics for optimum process results
To determine weight data, Keil Anlagenbau used, among other things, HBM’s AED 9301 analysis electronics. The AED9301 is connected to a programmable logical controller (PLC) via Profibus DP. Once the current weight data is analyzed by the PLC, it can be displayed centrally on a process display screen, if necessary. The AED9301 can be set up and calibrated from a PC or laptop via user-friendly HBM Panel 32 software.
PC-driven batching and mixing equipment
The plant diagram shows batching and mixing equipment consisting of a PC workstation, a PLC, a 1,000 liter mixer, three 250 liter feedstock tanks and a workstation for filling small components on a 30 kg manually-operated balance.
Raw materials and recipes are managed from the PC workstation. Captured production data is stored on the PC. The PC has a printer connected to it for producing batch reports, and a modem for remote diagnostics and maintenance.
The PC is connected to the PLC over an MPI interface. Also connected to the PLC via Profibus DP are five sets of AED9301 analysis electronics, a control panel located in the mixer section and another control panel located in the small components manual filling section. The control panel located in the mixer section is used to call up the next recipe due for processing and start it when needed.
The liquid components included in the recipe are batched into the 250 liter feedstock tanks and emptied into the mixer tank. At the manual filling section, small components are pre-weighed by hand according to the recipe and released into the mixer tank through a hopper. The finished batch is then packed in 200 liter canisters for forwarding to the next part of the production process. The 200 liter canisters are filled by starting a “batch draw-down” function on the mixer tank.