Case studies on agriculture

Idento Operations uses HBM load cells for intelligent feed systems

Idento from the Netherlands makes special measuring units for weighing feed quantities for pigs and cattle. Idento uses hermetically-sealed load cells from HBM for its measuring units, and they have turned out to be able to...

オーストラリア最大のワイン生産地で使用されるのは、HBM製ユニバーサルZ6ロードセル

湿度が高い上に高温になる加工済み材料 - オーストラリアの Accuweigh 社は、堆肥工場での過酷な条件に対応するため、HBMの計量技術に依存しています。

Weighing and batching electronics: The Bavarian State Research Center for Agriculture (LfL) relies on HBM weighing technology

Lab-based research studies for optimizing the methane yield and managing the process control of anaerobic digestion of renewable raw materials developed an automatic filling device that continuously loads the fermenter system...

Too much fertilizer? A globally unique test bench for investigation and analysis

Cemagref, the French Institute for Agricultural and Environmental Engineering Research is a specialist in spreading fertilizer at one of its nine sites in Montoldre. The equipment to chart the spread of the fertilizer as it is...

小麦と剥き殻の分離:品質管理にHBMの計量技術が使われています

穀物類は世界中で生産され、商品市場で取引され、複雑な経路をたどって加工業者へ引き渡されます。量はもとより、主としてはその生での状態の品質が価格を決めるファクターとなります。

Want to see your application here?

Share a case study of your HBM product with us!

Please contact us