reports in applied measurement

reports in applied measurement is an in-depth journal on measurement technology comprising articles submitted by independent authors.

RAM has a tradition going back to the mid-1960s.

It is edited by Dr. Martin Stockmann from the Institute of Mechanics at the University of Chemnitz, Germany. It is issued twice yearly in English and German exclusively on our website.

三軸テストセル内にある超高性能コンクリート(UHPC)における変形の進行を度量衡的に記録する

この論文では、 "三軸セル" 試験装置を使用することにより、静的荷重および動的荷重の両方において三軸強度を決定することが可能であることをご説明しています。

Numerical simulation of strain gages

This article describes how to apply numerical methods to determine the properties of the strain gages and then, by specifically modifying the material and geometric properties, to change the strain gages so that they meet certain...

Monitoring the Reichenbach and Albrechtsgraben viaducts

Normally, road bridges are visually inspected at regular intervals, in order to detect any defects and/or to decide whether additional rehabilitation might become necessary.

Identifying the material parameters of carbon fiber reinforced plastics with strain gages, taking transverse sensitivity into account

This article describes the process of identifying the material parameters of characteristic carbon fiber reinforced plastics (CRP).

reports in applied measurement


ISSN 1614-9912