전문기술관련 기사.
시장 리더의 경험을 통한 이점...
기본 지식, 적용 사례, 제품 정보 - 제조공정관리를 주제로 한 HBM의 다양한 기술관련 기사 및 보고서들.
T40B with rotational speed measuring system and reference pulse
There are countless incremental rotational speed measurement systems available on the market. However, these systems are intended solely for measuring rotational speed. Combining rotational speed and torque measurement in a...
Spoilt for choice: piezoelectric or strain gauge based force transducers?
Two principles have become dominant in force measurement: Piezoelectric sensors and strain gauge (SG) based force transducers. When is which principle appropriate?
새로운 응용분야로의 열쇠: 정밀도
효율적인 이용: S형 S2M 힘 변환기
HBM의 S2M과 같은 고정밀 변환기를 사용하여 다양한 장점을 누리세요. 높은 기계적 보존성을 가지도록 설계되어 0.02 정확도 등급으로 힘 측정 체인을 가능한 센서들을 제공합니다. 또한, 다른 측정 작업들을 위해 변환기들을 유동적으로 이용할 수 있는 점은 주요 경제성 장점입니다.
Force shunt measurement using CFW piezoelectric force washers
The measuring chain's sensitivity varies depending on the pre-stressing device's design. For example, when HBM's CPS set of pre-stressing elements is used, the CFW piezoelectric force washers' sensitivity is reduced by 7-12 %....
포스 션트에서의 포스 측정: 실제로 세 가지 방법이 사용되고 있다.
Sometimes it is of advantage to measure force in the force shunt. This article presents three methods used for measurement in the force shunt.
How does a strain gauge-based force transducer work?
The functionality, benefits and special characteristics of strain-gauge force transducers: This technical article provides the perfect introduction to the topic.
High accuracy is high efficiency
Why particularly accurate force transducers enable new application areas
FDT technology for amplifiers
In 2003, a number of prestigious companies in the automation sector established the FDT Group, in order to create a common communications and configuration interface for field devices in automation technology. We now have...
New HMI Software Solutions for Process Monitoring: A Modular System
Operability and functional control - it is just these requirements that HBM addresses with the new HMI software solutions of FASTpress Suite.
측정 결과를 가장 효율적으로 얻는 방법:
The most important cost saving potentials for your test and measurement equipment are found in installation and operation