Case Studies on Torque Measurement

HBM is considered the worldwide reference in torque measurement technology. In test benches, calibration tasks and production monitoring, HBM torque transducers guarantee reliable results—for example, in the automotive and shipbuilding industry, in the energy industry for measuring torque at generators, and in many other fields of applications.

토크 측정에 관한 적용사례 보고서

HBM torque transducer in headwind vehicle developed by University of Stuttgart

Team InVentus from the University of Stuttgart, equipped with a T22 torque transducer from HBM, was once again able to successfully participate in the Aeolus Race.

Testing an actuator with T20WN: Article in 'Lufthansa Magazine'

Lufthansa Magazine reported in its edition from November 2013 about an actuator testing application using HBM's T20WN torque sensor.

올바른 테스트 장비를 선택하면 고효율 전기 자동차 생산에 도움이 됩니다.

고효율 전기 자동차의 개발과 생산에는 많은 연구가 필요합니다. 더 중요한 테스트 분야 중 하나는 토크 측정입니다.

How Torque Transducers Help Optimize Hybrid Drivetrains for Buses and Trucks

Automotive OEMs commonly house test stands or special facilities to develop, characterize, and test car engines. As hybrid technology plays an increasing role in vehicle designs, OEMs increasingly use such facilities in the...

New generation of high-speed engine dynamometers

The Australian company Dyno Dynamics is working on a new generation of high-speed engine dynamometers. The heart of the dynamometers: The T40B torque transducer from HBM.

EtherCAT-capable test stand for electric motors - with TIM-EC

Dynosens needed an interface to connect the T40B torque transducer to an EtherCAT fieldbus. The solution: TIM-EC from HBM.

Accurate measurement data for Sisu Axles’ product development with HBM T40 torque transducers

For developing more durable and more capable axles, Finnish manufacturer Sisu Axles equipped its new test stand with torque transducers from HBM.

HBM on the test bench: Allison Transmission puts HBM to the test

Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...

Better driving thanks to PME

For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...

T10F Torque transducer ensures optimization of INVT control algorithm

The Chinese company, INVT, has utilized HBM’s T10F torque transducer and MP60 amplifiers to measure torque and speed of an electric motor controlled by a variable frequency drive (VFD) in order to optimize performance.

Displaying results 1 to 10 out of 21

1

2

3

Next >