토크 측정에 관한 기술관련 기사
T40B with rotational speed measuring system and reference pulse
There are countless incremental rotational speed measurement systems available on the market. However, these systems are intended solely for measuring rotational speed. Combining rotational speed and torque measurement in a...
Fieldbus based measurement technology for digital transmission of torque and rotational speed in test benches
Torque and rotational speed measurement equipment must be compatible with the increasing number of fieldbus based systems. Read this article to learn how T40B and T40FM digital torque transducers meet these requirements.
Measuring torque in wind energy applications
There is no power generation without rotation, hence, there is no power without angular speed and torque: This applies to wind energy in particular. This article highlights the importance and significance of measuring torque in...
The right fit for your torque transducer
Correct torque application to the transducer is crucial for measuring torque. We show you what to keep in mind when selecting a fit.
Checking HBM torque flanges using the shunt signal and the zero point
Torque transducers need to be calibrated before being put into operation. A practicable method is to determine the characteristic curve of the transducer using a zero point value and a second reference value based on the shunt...
Use of torque flanges in power generation plants
Power generation plants need to be economical and eco-friendly. To determine the efficiency of such plants, drive power needs to be measured. However, which method is most suitable? Read this technical article to learn how to...
토크 어플리케이션을 위한 커플링과 마운팅 부품 - 선택 가이드
어떤 커플링이 적합한가?
토크 플랜지는 작고 불확실한 측정이 가능한 정밀한 센서입니다. 그러나, 이를 측정하기 위해서 특별한 요구조건을 만족시켜야 합니다. 각각의 구동렬 (Drive train) 사이에서 결합이 어긋난 결과로 인해 센서에 발생하는 기생 부하 영향을 최소화하는 것이 가장 중요합니다. 측정 플랜지에 설치된 샤프트 끝의 반경 병렬 옵셋(radial parallel offset)은 센서에...
연소 엔진의 큰 드라이브상의 동력 측정
There are different ways to measure the power of large drives with combustion engines. Learn how direct power measurement in the drive train reduces the uncertainty of measurement, by contrast with indirect measurement on the...
저공해 선박 드라이브. 토크 트랜스두서는 효율성을 최대화 할 수 있도록 도와줍니다.
측정 기술이 드라이브 트레인으로 통합하는 것은 선박 엔진 제어에 효율성을 제공 합니다. HBM 토크 트랜스두서는 선박의 추진력의 경제성을 최적화하고 환경을 보호하는 것을 도와 드립니다.