항공우주 실험 적용사례 보고서
Bucher Leichtbau uses HBM test and measurement technology to test airworthiness of galleys
Bucher Leichtbau AG, Switzerland, is a leading manufacturer of galleys and cabinets installed in passenger aircraft and therefore places its trust in stringent testing of its modules to ensure their airworthiness. In the test...
Advanced lightning warning system protects spacecraft launches at Kennedy Space Center
Using HBM transient recorders and digitizers, HBM has designed a lightning monitoring system for Kennedy Space Center in Florida. The system enhances the safety of operations such as the launching of rockets by ensuring that the...
Static component testing of a drive module with MGCplus
The BEPICOLOMBO mission: The European Space Agency (ESA) and the Japanese Space Agency ISAS/JAXA want to explore Mercury – with a drive module and two separate space probes that will orbit around the planet.
HBM 은 현대 상용 항공기를 위한 안전한 기체 조립을 제공합니다.
점차 오늘날 현대 상용 항공기의 건설은 유리섬유복합관(GRP)이나 글레어(GLARE)와 같은 혁신적인 복합 재료의 사용을 포함합니다. 조립하는 동안 이러한 재료를 다루는 것은 항공기 제조업체의 새로운 과제입니다. 그러므로 HBM은 생산하는 동안 최적화된 공정 안정성과 최적화된 제조 비용 및 런타임을 위해서 공정 모니터링을 위한 자동화 제조 컨셉에서 혁신적인 해결책을 지원합니다.
조립과정에서 기체...
Latest Lynx lands safely following development tests
AgustaWestland has conducted a series of tests on the undercarriage of the future Lynx naval helicopter using HBM’s data acquisition equipment to ensure superior operational landing performance.
MGCplus와 catman®Enterprise를 이용한 항공우주 분야의 구조 및 기초 실험
- Static or dynamic full-scale structural testing
- Component stress or functionality testing
- Fatigue trend monitoring and assessment
- Static load, fatigue or durability stress analysis
- Ironbird functionality and mechanical testing
- Landing gear drop tests
- Environmental and thermal testing
- Wind tunnel and aerodynamic testing