응용 보고서
Serving a greener automotive industry
The demands on energy efficiency and the CO2 balance of motors are constantly increasing. A manufacturer of water, oil and vacuum pumps for thermal engines therefore decided to use a complete solution from HBM.
Testing of electric and hybrid cars: HBM, a key partner for the French company, GreenMot
Tests on electric motors present a new challenge when it comes to measurement. French testing company GreenMot has opted for HBM's innovative eDrive testing solution.
HBM on the test bench: Allison Transmission puts HBM to the test
Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...
Better driving thanks to PME
For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...
Reducing the cycle time with FASTpress when assembling cylinder heads
In combustion engines, valve seats and valve guides are subjected to special loadings. There are thermal loads as well as mechanical loads, produced by the ignition pressure or by the valve disk coming down hard when closing....
Volvo Construction Equipment (CE): Making loaders more fuel-efficient with toughest tests - and SoMat eDAQ data acquisition
Volvo Construction Equipment (CE) uses HBM's SoMat eDAQ test system to help it test loader prototypes under extreme conditions.
Electromobility in the fast lane: Efficiency enhancement for the drive of the future
Electrically-driven vehicles have until now been living on the sidelines. But due to ever decreasing oil supplies, increasing fuel prices and a growing environmental awareness, the future belongs to electromobility. In order to...
교통 흐름상의 반응 시간: HBM 기술을 활용하는 혁신적 테스트 방법
교통 흐름에 있어 반응 시간은 종종 1/1000 초 단위의 문제로 귀결됩니다. 위험한 상황에서 차량 휠을 어떻게 반응하게 할까요? 얼마나 빨리 브레이크를 밟게 될까요? 연구실에서 재현하기에는 매우 어려운 상황들입니다. HBM 계측 기술의 도움을 받아, 스위스 엔지니어 Mauro Balestra는 실제 교통 흐름 조건 하에 테스트 차량에 위험한 상황들을 재현하는 방법을 개발하였습니다.
Efficient vehicle drives with measurement technology in the original component
Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...
Aluminum alloy wheels - tested with QuantumX MX410 data acquisition modules
Shorter development times - this is the aim of all technology companies worldwide. BORBET, the world's leading manufacturer of aluminum wheels shows how it is done: Using a smart system of efficient tests. Always on board: HBM...