HBM launches the latest version of Perception data acquisition software
HBM has released version 6.0 of its leading Perception data acquisition software. Perception integrates multi-platform hardware control, live display, data acquisition, review, analysis, report generation and data export in one package.
Darmstadt – HBM has released version 6.0 of its leading Perception data acquisition software. Perception integrates multi-platform hardware control, live display, data acquisition, review, analysis, report generation and data export in one package. It has been designed from basic principles ensuring that it is easy to use while allowing control of both small and large-scale systems.
This latest version adds live FFT capabilities to the HBM Genesis HighSpeed product family, allowing users to visualize signals simultaneously both in the time and the frequency domain. Because it is PC-based, it is usable with any Perception-controlled DAQ system, such as the portable GEN5i, GEN7t or GEN16t rack mainframes, and LIBERTY.
FFT is particularly useful, especially for customers that are just starting out in frequency domain analysis, because of its ease of use and high flexibility. For example, FFT can be enabled for transferring signals currently shown in the time domain to the frequency domain with a single click. The basic FFT option al-lows a choice of window lengths of up to 1 million samples, four different weighting filters, and analysis functions such as FFT Spectrum, Auto Power Spectrum or Power Spectral Density. For critical settings the software includes readily-accessible help ensuring users make the right choice for the best results.
Perception also provides powerful customization tools. Customer-specific plug-ins created with the Customer Software Interface (CSI) are fully integrated in the Perception operator interface so that user-specific and automated tasks can be included in the workflow. Close integration with Microsoft Office allows the user to easily transfer tables, displays and results into Word or Excel.
HBM's patented StatStream technology allows large data sets – even with Gigabytes of data – to be handled, reviewed and analyzed in just a few seconds. With StatStream, several parallel, reduced data streams are produced in real-time during the measurement, and saved with the raw data. If, for example, a 10-Gigabyte data set is displayed on-screen, this display is then generated from a reduced data set.
Perception is HBM´s high-end software to control the Genesis HighSpeed product family. This ranges from rugged data acquisition systems with sample rates of 100 kS/s to the top-end GEN DAQ series with sample rates up to 100 MS/s.
Further information at: www.hbm.com/highspeed