称重技术的应用报告
Idento Operations uses HBM load cells for intelligent feed systems
Idento from the Netherlands makes special measuring units for weighing feed quantities for pigs and cattle. Idento uses hermetically-sealed load cells from HBM for its measuring units, and they have turned out to be able to...
Optimal dosing always in view: RTN installation modules in a new CEMEX Austria binding material silo
In order to ensure optimal mixing and dosing of the material anhydrite flow, CEMEX Austria is using HBM weighing technology for their new binding material silo.
采用 HBM 技术进行矿山机械称重和重心测量
成立于1953年,塞尔维亚 Kolubara Metal Vreoci 公司是Kolubara 大型工矿业集团的子公司。专门从事采矿设备生产,设备维护,修理,以及用于采矿业中使用的各种工程机械。
四周无需充电: 无线移动衡器展示出其杰出的耐久性
来自 S+P Wägetechnik GmbH 最新的无线衡器连续4周工作 - 而无需充电。 以前由于电池的限制,其只能工作数天。成功的诀窍来自 S+P 的精巧设计和来自 HBM 的技术和经验。
精确且可靠 - Straightpoint 信赖 HBM 应变片
自从 负载测试专家 Straightpoint (英国) 使用 HBM 应变片 以来,故障率大幅降低。
精确,可靠,优质的服务 - 了解为何 Straightpoint 信赖 HBM 产品.