Artículos técnicos sobre test y medida
Menores tiempos en desarrollo gracias a ensayos más eficientes
La técnica de medición de nueva generación de la industria automovilística contribuye a presentar más rápidamente nuevos modelos en el mercado
Conecte y empiece a medir: – TEDS: Plug and Measure utilizando identificación electrónica de transductores (TEDS)
Plug and Play es un concepto largamente conocido en la tecnología PC. Ahora ha comenzado a introducirse en la tecnología de medición y ensayo profesional. HBM ha liderado activamente el desarrollo de la tecnología TEDS...
On-Site Loading Test of Tunnel Lining Segments in Barcelona
Read how scientists from the Technical University (UPC) carried out loading tests during the construction of the “L9” two-level subway line in Barcelona, Spain. The engineers used a very complex test procedure for analyzing the...
All the president's helicopters: Data acquisition system for rotor blade testing at AgustaWestland
The key criteria of the next generation of presidential helicopters was to ensure the safe transportation of the President of the United States of America, and effectively create an 'Oval Office in the sky'.
A new type of transducer for accurate and dynamic pressure measurement up to 15,000 bar using foil strain gage types
Applications in the ultra-high pressure range are on the move forward. Of particular interest is the manufacturing of diesel injection components such as nozzles and rails.
Displaying results 11 to 15 out of 15