エネルギー工業
HBM - エネルギー工業の最良のパートナー
エネルギー需要は世界的かつ継続的に高まっています。そしてその高まりにより、最適な性能を発揮する状況下において、確実な稼働構成をもった設計や構造に対する要望も高まり続けています。 HBMは、再生可能エネルギーや原子力、オイルやガスを含む全てのエネルギーセクターで、構造的解析と安定した稼働を支えるという両方に適用できる、広範囲にわたる製品を開発しています。これにより、HBMはアプリケーションが陸上であれ海上であれ、エネルギー工業にとっての理想的なパートナーとなっています。
HBMのアプリケーション概要を知るにはこちらから:
Typical applications include:
Measurement data acquisition in high-voltage areas

- Solutions for impulse tests, high-voltage tests.
Tests in high-voltage areas, such as lightning and switching impulse tests place extraordinary demands on the test equipment used. HBM high-voltage products enable reliable measurement data acquisition thanks to electrical isolation, electromagnetic immunity and many other features. The devices have been tried and tested and are used in thousands of applications worldwide. Typical applications include:
- Testing of switching systems, such as switching devices and fuses
- Lightning impulse tests, for example, for testing transformers, surge protectors, isolators and switching systems
- Determination of current zero-crossing.
High-voltage data acquisition solutions
Durability tests on components

- Tests on a blade of a wind turbine with optical strain gauges from HBM
Many structures in the energy industry are subject to high loads: pipelines, power poles or the foundations and towers of wind turbines. Experimental stress analysis is the ideal method to determine stress in materials.
HBM offers a wide range of strain gages and measuring amplifiers as well as professional catman®AP software for experimental stress analysis.
Especially useful for applications in the energy industry: the many possibilities of optical measurement technology using fiber Bragg sensors—measurement with light. Electromagnetic influences can no longer affect the measurement results.
Torque efficiency tests on generators

- T10FH torque transducer from HBM
The demands on the efficiency of generators in all kinds of power plants are increasing dramatically.
Cost pressure and more stringent environmental regulations require knowledge of specific characteristic values reflecting the performance of your generators. HBM is the global market leader in torque measurement—and provides a range of powerful analog and digital torque transducers.
HBM's precise and robust torque transducers are the better choice—in particular in comparison to the indirect torque measurement methods widely used so far.
Weighing technology applications for the energy industry

- HBM weighing module on a gas tank
Whether in gas tanks, with raw materials or in nuclear power plants: Load cells are used in many applications in the energy industry.
HBM's wide range of load cells and weighing indicators offers the right solution for every application—be it for tank weighing or in dynamic weighing processes.
Even in the demanding field of uranium enrichment with high temperature fluctuations, HBM's RTN load cells provide precise and reliable measurement results.
System design, test automation

- HBM nCode fatigue and durability software
Test strain on your systems and structures already in the design phase!
HBM nCode's professional software solutions enable you to carry out "virtual tests" even before starting the production of prototypes. Save costs and increase your efficiency by performing durability and fatigue analyses already in the development phase. Many users from the energy industry, especially from nuclear and wind energy, rely on HBM nCode solutions.
HBM nCode Software Solutions
Wind energy applications
In Wind energy there are versatile applications such as the monitoring of the wind load in the blades of wind turbines in order to increase reliability and availability of wind turbines. The same system can be used to protect the wind turbine from high winds by stopping the machine and turning the blades into a safe position.
Another example for applications in wind energy is power measurement. The mechanical power e.g. of generators needs to be measured accurately with HBM high precision torque transducers according to the standard IEC 60034.
Wind turbine testing with HBM
エネルギー工業でのアプリケーション
Chinese develop enhanced diesel engine monitoring system for nuclear power plants
Chinese engineers have developed an engine monitoring system based on HBM’s GEN2i data acquisition equipment to ensure standby diesels meet enhanced nuclear safety regulations.
HBMの計測技術により実現した耐用年数の長さと停止時間の短さ
HBMは、最新の計測技術を使用した風力エネルギーのように、非常に将来性の高い成長マーケットをサポートしています。センサからソフトウェアまでを含むHBM製の計測技術を使用した風力発電プラントでは、その効率を向上させるために完全なソリューションを必要とします。
Uranium isotope enrichment process: RTN load cells impress under extreme conditions
RTN load cells can demonstrate their strengths even in the technically extremely demanding isotope enrichment process.
絶縁による計測結果の向上
計測結果の質には、いくつかの要素が影響を及ぼします。一部のアプリケーションでは、電気的な絶縁が大幅な改善のカギを握っています。この資料では、様々なトポロジー(接続形態)を示してそれぞれの利点や限界について考察します。
テストスタンド上のHBM計測技術 - 水タービン内でのダイナミックトルク計測
トルクをより確実に計測するにはどうしたらよいでしょうか?ある有名な水タービン用テストスタンド製造メーカーでは、ある新しいコンセプトに信頼を寄せています。力変換器を使用し、復元力を通して間接的に計測する代わりに、ずっと優れた結果を提供してくれるT12デジタルトルク変換器を取り付けるという方法です。そうすることで、高性能の計測技術によって水力発電における効率が大幅に向上します。
Pictures by Jan Ortgies & Gernot Grundey - Photocase
Solutions for wind turbine testing
HBM offers many professional solutions for tests in the wind energy industry—during the development of plants, but also for structural tests of existing wind turbines.