계측 및 실험 분야의 적용사례 보고서
Load monitoring in the Olympiahalle arena in Munich
Concerts nowadays, particularly when they involve pop music, are becoming more and more extravagant. Accordingly, the equipment used by the artists for light and sound is large and heavy. As there is a limit to the maximum load...
One for all - Universal hydraulic test bench with secondary control
Until now, hydraulic test benches were designed for special tasks or products. Although the individual components are already tested, the interaction between individual pumps and control systems can only be tested in the machine...
Advanced lightning warning system protects spacecraft launches at Kennedy Space Center
Using HBM transient recorders and digitizers, HBM has designed a lightning monitoring system for Kennedy Space Center in Florida. The system enhances the safety of operations such as the launching of rockets by ensuring that the...
Setting new records at sea: The fastest sailing boat in the world uses QuantumX
Alain Thébault of France has been pursuing his dream of building the fastest sailing boat in the world for decades. To make this dream a reality, Thébault has consistently relied on leading-edge technologies. When bordering on...
Static component testing of a drive module with MGCplus
The BEPICOLOMBO mission: The European Space Agency (ESA) and the Japanese Space Agency ISAS/JAXA want to explore Mercury – with a drive module and two separate space probes that will orbit around the planet.