Load application in load cells - Tips for users
Correct load application on the load cells is a prerequisite for precise weighing results. Be it load direction, support structure or mounting aids – load application is influenced by multiple factors.
How does a bending beam load cell work?
Bending beam load cells are the most widely used types of load cells. Read this article to learn more about the benefits and properties of bending beams.
Legal-for-trade weighing systems in open automation applications
Weighing technology plays an important role in many areas of logistics and in commerce. For example, legal-for-trade, automatic weighing instruments are often used when bulk materials are measured out or loaded.
Automatic weighing instruments for legal-for-trade applications: requirements and directives
Weighing technology plays an important role in many industrial applications, for example in bulk material logistics. Depending on the application, different types of automatic weighing instruments are used.
위생적인 설계는 의무적입니다.
식품 산업분야를 위한 로드셀
최근 수십 년간 식품생산에서 몇몇 근본적인 변화가 있었습니다. 요즘 소비자들은 방부제가 없고 가능한 한 신선한 식품을 요구합니다. 또한 세계화로 인하여, 몇몇 제품들을 만들기 위해 장시간 운반을 해야 합니다. 이러한 개발은 생산하는 동안 더욱 엄격해진 위생 조건의 결과입니다. 때문에 그 결과로 만들어진 제품들에 세균이 없거나 아주 적은 양이 있다면 충분히 오랜 시간 상하지 않게...