Relatórios de aplicação
Load testing on the Ponte della Costituzione in Venice
The Ponte della Costituzione is designed by the Spanish architect Santiago Calatrava and became the fourth bridge over the Grand Canal in Venice when it was inaugurated in September 2008. HBM Italy worked with Verona-based Veneta...
Monitoring El Giraldillo in Seville
El Giraldillo is a 5 meter high bronze sculpture weighing 2000 kilos, which crowns the top of the tower of La Giralda, the Seville Cathedral. This 98 meter high tower is a former Almohaden minaret and at the time of its erection...
Tecnologia e serviço HBM para a construção do primeiro parque eólico marítimo alemão
Nestes tempos de preços elevados e de crescente consciência quanto ao cuidado com o meio-ambiente, uma eficaz e não-poluente produção de energia elétrica adquire uma importância cada vez maior aos olhos do usuário.
Medição de stress residual no método de perfuração (em inglês)
SINT Technology is an Italian firm located in Florence, Italy. The company, in partnership with HBM, produces and develops the MTS 3000, an automatic system for measuring residual stresses by the hole-drilling method.
Optical sensors for lightweights
Modern lightweight materials are increasingly being used in aerospace applications and in other branches, such as traffic and construction engineering, mechanical engineering and the energy business. Fiber composite technology in...