Artigos técnicos
Beneficie-se de nossa experiência.
Conhecimento fundamental, exemplos de aplicações, informação do produto - várias publicações da HBM referentes à monitorização de processos.
Checklist: 5 decision-making criteria for amplifiers in production and industrial test benches
The use of amplifiers in production is an essential part of your quality assurance process. What are the decision-making criteria you should take into account when selecting a new industrial amplifier? Is the system you are...
Measuring forces in the force shunt: Three methods used in practice
Sometimes it is of advantage to measure force in the force shunt. This article presents three methods used for measurement in the force shunt.
Force transducers based on strain gauges
Force transducers based on strain gauges have a so-called spring element or loaded member where the forces to be measured are applied. The spring element deforms and strain is produced on the surface. The task of the spring...
High accuracy is high efficiency
Why particularly accurate force transducers enable new application areas
FDT technology for amplifiers
In 2003, a number of prestigious companies in the automation sector established the FDT Group, in order to create a common communications and configuration interface for field devices in automation technology. We now have...