Artigos técnicos
Torque measurement in wind turbines - as relevant today as it was in the past
This article clearly shows how important torque measurement in wind turbines was years ago and still is today. There is no power generation without rotation, hence, there is no power without angular speed and torque.
Centrifugal acceleration in torque measurement - often underestimated, however, very effective
Centrifugal accelerations in torque measurement are very high. The caused forces require correspondingly safe structures.
Which fit is the right one?
An explanation of the significance of ISO fits to standard shafts and holes
Checking HBM torque flanges using the shunt signal and the zero point
Users often ask whether they may continue using a torque flange that has not been in use for an extended period of time.
The use of torque flanges in power generation plants
Power generation plants need to be economical and eco-friendly. To determine the efficiency of such plants, drive power needs to be measured. However, which method is most suitable? Read this technical article to learn how to use...